Code Exchange
  • Technologies
  • More
Code Exchange
Polls What programming language should EE's learn first?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Code Exchange to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: bluescreen
  • Date Created: 13 Feb 2014 4:26 AM Date Created
  • Last Updated Last Updated: 11 Oct 2021 3:01 PM
  • Views 11307 views
  • Likes 0 likes
  • Comments 88 comments
Related
Recommended

What programming language should EE's learn first?

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • johnbeetem
    johnbeetem over 12 years ago +2
    Oh goodie, language wars! Personally, I think C and C++ are terrible first programming languages. C is a great language for writing compact code that maps directly into machine language, but for teaching…
  • e14 Contributor
    e14 Contributor over 12 years ago +2
    Ruby! It's python's beautiful little sister.
  • e14 Contributor
    e14 Contributor over 12 years ago +2
    Very important distinction here is that the question specified "EE", not "CS"! EEs should learn C first, but not bother with C++ so much. C compilers are available for every processor made and by learning…
Parents
  • toxxn
    toxxn over 11 years ago

    I have been self-teaching myself programing languages for about 9 years (Since I was 14) and I started with what I believe was the easier of the languages first and then slowly went down the list.

     

    HTML, CSS, PHP, Java/ Javascipt - I started off with these because they are all pretty simple and easy to learn. All of which are also used in web development. I started with HTML and CSS first because I believe they are the easiest to learn and both are great languages for anyone to first start off with. I then went on into PHP, Java and Javascript. Java alone is used in so many different applications that it is almost a must know.

     

    Python, C, C++ - Like Java, C and C++ are used in so many different applications they are almost a must know, albeit in my opinion they are a little more difficult especially if you are self taught like myself. I included Python with C and C++ because I started learning these three pretty much around the same time because of Linux. Although other languages are used with Linux, these three are the main ones.

     

    BASIC - I don't really want to talk about BASIC.

     

    Other, there are so many other languages out there that "other" is a lot easier to use, rather than listing them all. This list in this poll pretty much covers the most common programming languages however, so I won't really go any further into which ones I have learned.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 11 years ago in reply to toxxn

    Very good and from a self taught expert, also. Python should be separate since it can be interpreted line by line. It even alows display of computed values without Print statements.

    Just my two cents worth

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • toxxn
    toxxn over 11 years ago in reply to clem57

    I agree, however the only reason I included it with C/C++ is because I started learning them around the same time because that is when I also started messing with Linux for the first time. Since then I have used C/C++ for many more applications other than Linux.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • toxxn
    toxxn over 11 years ago in reply to clem57

    I agree, however the only reason I included it with C/C++ is because I started learning them around the same time because that is when I also started messing with Linux for the first time. Since then I have used C/C++ for many more applications other than Linux.