Code Exchange
  • Technologies
  • More
Code Exchange
Polls What programming language should EE's learn first?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Code Exchange to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: bluescreen
  • Date Created: 13 Feb 2014 4:26 AM Date Created
  • Last Updated Last Updated: 11 Oct 2021 3:01 PM
  • Views 11296 views
  • Likes 0 likes
  • Comments 88 comments
Related
Recommended

What programming language should EE's learn first?

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • johnbeetem
    johnbeetem over 12 years ago +2
    Oh goodie, language wars! Personally, I think C and C++ are terrible first programming languages. C is a great language for writing compact code that maps directly into machine language, but for teaching…
  • e14 Contributor
    e14 Contributor over 12 years ago +2
    Ruby! It's python's beautiful little sister.
  • e14 Contributor
    e14 Contributor over 12 years ago +2
    Very important distinction here is that the question specified "EE", not "CS"! EEs should learn C first, but not bother with C++ so much. C compilers are available for every processor made and by learning…
Parents
  • nick123
    nick123 over 11 years ago

    You should not try assembly until your a programming expert, Its very complicated, I recommend python or C/C++

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • johnbeetem
    johnbeetem over 11 years ago in reply to nick123

    Nick Gallagher wrote:

     

    You should not try assembly until you're a programming expert.  Its very complicated, I recommend python or C/C++

    IMO assembly language is very simple.  You have very simple instructions that do very simple things.  It's when you combine instructions that things get complicated image  It's kind of like circuit theory.  Basic circuit elements like resistors and capacitors are simple, but when you put them together the number of simultaneous equations quickly overwhelms you.  (I do believe in Kirchhoff's Laws, I do I do I do.)

     

    Personally, I think one should learn ASM before C.  In many ways C is a portable assembly language, and at run time programs fail at the machine language level.  If you haven't experienced (or preferably mastered) assembly language, you'll have a dreadful time understanding some bugs like clobbering the run-time stack.

     

    Also, if you're going to write a compiler IMO you should be one for a while first so you know the challenges first-hand.

     

    JMO/YMMV

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 11 years ago in reply to johnbeetem

    @nick123

    Write macro's to remove some of the repetitive coding! Just like creating libraries for C code.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • johnbeetem
    johnbeetem over 11 years ago in reply to clem57

    Clem Martins wrote:

     

    Write macro's to remove some of the repetitive coding! Just like creating libraries for C code.

    I once wrote a recursive macro in PDP-11 Macro-11 just to prove to myself that I could do it.  It generated all permutations of a sequence of data bytes.  5 bytes took 1 minute to assemble.  6 bytes took 6 minutes to assemble.  Generating them at run time was instantaneous.  image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • nick123
    nick123 over 11 years ago in reply to johnbeetem

    Thats true, But there are many types of assembly. I'm learning 16-bit real mode assembly. And, It's pretty hard for me.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • nick123
    nick123 over 11 years ago in reply to johnbeetem

    Thats true, But there are many types of assembly. I'm learning 16-bit real mode assembly. And, It's pretty hard for me.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • michaelkellett
    michaelkellett over 11 years ago in reply to nick123

    Is there any particular reason why - it seems a bit odd because mostly one codes in assembler for the best possible optimisation so why not use a 32 bit processor and be quicker anyway ?

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • johnbeetem
    johnbeetem over 11 years ago in reply to nick123

    Nick Gallagher wrote:

     

    Thats true, But there are many types of assembly. I'm learning 16-bit real mode assembly. And, It's pretty hard for me.

    Which processor?  Ease of programming in ASM varies widely with the instruction set.  I did most of my ASM for PDP-11, which is a very clean 16-bit architecture.  The Motorola 68000 is based on PDP-11, so it's likewise pretty clean though you do have to distinguish between address and data registers.  x86 is a nightmare, since it's source-code compatible with Intel 8008 :-)  ARM is a decent ASM, but if you look at the instruction set coding it's a dog's breakfast with each architecture version fitting new instructions into the holes of the previous versions.  If you like railroad time schedules with lots of footnotes, you'll love the ARM quick-reference guide.

     

    I've been intrigued by the TI MSP430 instruction set.  It's clearly based on PDP-11, with some RISC concepts tossed in.  Looks very clean.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 11 years ago in reply to johnbeetem

    TI MSP430 looks MIPS like to me...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • nick123
    nick123 over 11 years ago in reply to johnbeetem

    I think the processor was an  8086.