Connector Technology & Design
  • Technologies
  • More
Connector Technology & Design
Blog Phoenix Contact Introduces SKEDD Direct Connectors with Crimp Connection
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Connector Technology & Design to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: rscasny
  • Date Created: 16 May 2020 12:50 AM Date Created
  • Views 1861 views
  • Likes 6 likes
  • Comments 2 comments
  • skedd direct connectors
  • phoenix contact
Related
Recommended

Phoenix Contact Introduces SKEDD Direct Connectors with Crimp Connection

rscasny
rscasny
16 May 2020

Phoenix Contact introduced its new double-row direct connectors with crimp connection. The CDDC 1,5 and CDDC 2,5 product series are ideal for applications with a high contact density.image

 

SKEDD is a mounting technology for connecting PCB connectors directly to the PCB via through-contacted bore holes. Mounting is tool-free and an additional header is not required. Body-bound rivets on the side of the connector ensure a reliable and vibration-resistant connection.

 

SKEDD direct plug-in technology combines the advantages of two established mounting technologies – press-in technology and direct plug-in connection. Due to the high mounting force, a gas-tight connection is established between the contacts and PCB in the case of press-in technology. However, this mounting type is not suitable for reversible connections.image

 

In contrast, direct plug-in connection requires contact pads on both sides of the PCB and is therefore only used for board-to-board or wire-to-board connections on the edges of the PCB. Innovative SKEDD direct plug-in technology now enables reversible connections that can be easily plugged in and ensure long-term stability while providing maximum flexibility for the PCB layout.

 

SKEDD contacts from Phoenix Contact consist of two pairs of legs that adapt to the diameter of the through-contacted PCB holes when inserted. This increased stability of the contact ensures a very stable connection between the connector and PCB, even in the event of mechanical strain such as vibrations.

image

The normal contact force of the direct connectors is designed in such a way that a safe electrical connection is ensured yet the connector can still be disconnected from the PCB during maintenance.

  • Sign in to reply

Top Comments

  • dougw
    dougw over 6 years ago +1
    This looks interesting - The idea sounds like a time saver and they seem to have nailed it but it will still take some convincing that it can take cable stresses.
  • shabaz
    shabaz over 6 years ago +1
    They look awesome, been in the back of my mind for ages to try them out on a board. I got a mini-demonstration of another SKEDD part in the range (push-fit wire instead of wire crimp) at an exhibition…
Parents
  • shabaz
    shabaz over 6 years ago

    They look awesome, been in the back of my mind for ages to try them out on a board. I got a mini-demonstration of another SKEDD part in the range (push-fit wire instead of wire crimp) at an exhibition, recorded here, but the crimp 1,5 version looks smaller which is great:
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
  • shabaz
    shabaz over 6 years ago

    They look awesome, been in the back of my mind for ages to try them out on a board. I got a mini-demonstration of another SKEDD part in the range (push-fit wire instead of wire crimp) at an exhibition, recorded here, but the crimp 1,5 version looks smaller which is great: