Connector Technology & Design
  • Technologies
  • More
Connector Technology & Design
Forum USB简述
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Connector Technology & Design to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 127 subscribers
  • Views 303 views
  • Users 0 members are here
Related

USB简述

YYD
YYD over 15 years ago

不过直到近期,它才得到广泛地应用。从1994年11月11日发表了USB V0.7版本以后,USB版本经历了多年的发展,到现在已经发展为3.0版本,成为目前电脑中的标准扩展接口。目前主板中主要是采用USB1.1和USB2.0,各USB版本间能很好的兼容。USB用一个4针(USB3.0标准为9针)插头作为标准插头,采用菊花链形式可以把所有的外设连接起来,最多可以连接127个外部设备,并且不会损失带宽。USB需要主机硬件、操作系统和外设三个方面的支持才能工作。目前的主板一般都采用支持USB功能的控制芯片组,主板上也安装有USB接口插座,而且除了背板的插座之外,主板上还预留有USB插针,可以通过连线接到机箱前面作为前置USB接口以方便使用(注意,在接线时要仔细阅读主板说明书并按图连接,千万不可接错而使设备损坏)。而且USB接口还可以通过专门的USB连机线实现双机互连,并可以通过Hub扩展出更多的接口。USB具有传输速度快(USB1.1是12Mbps,USB2.0是480Mbps, USB3.0是5 Gbps),使用方便,支持热插拔,连接灵活,独立供电等优点,可以连接鼠标、键盘、打印机、扫描仪、摄像头、闪存盘、MP3机、手机、数码相机、移动硬盘、外置光软驱、USB网卡、ADSL Modem、Cable Modem等,几乎所有的外部设备。

  USB接口可用于连接多达127个外设,如鼠标、调制解调器和键盘等。USB自从1996年推出后,已成功替代串口和并口,并成为当今个人电脑和大量智能设备的必配的接口之一。

  USB各版本区别版本最大传输速率速率称号最大输出电流协议推出时间USB1.01.5Mbps(192KB/s)低速(Low-Speed)500mA1996年1月USB1.112Mbps(1.5MB/s)全速(Full-Speed)500mA1998年9月USB2.0480Mbps(60MB/s)高速(High-Speed)500mA2000年4月USB3.05Gbps(640MB/s)超速(Super-Speed)900mA2008年11月