Connector Technology & Design
  • Technologies
  • More
Connector Technology & Design
Forum USB应用
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Connector Technology & Design to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 127 subscribers
  • Views 290 views
  • Users 0 members are here
Related

USB应用

YYD
YYD over 15 years ago

随着计算机硬件飞速发展,外围设备日益增多,键盘、鼠标、调制解调器、打印机、扫描仪早已为人所共知,数码相机、MP3随身听接踵而至,这么多的设备,如何接入个人计算机?USB就是基于这个目的产生的。USB是一个使计算机周边设备连接标准化、单一化的接口,其规格是由Intel(英特尔)、NEC、Compaq、DEC、IBM(商业机器公司)、Microsoft(微软)、Northern Telecom联系制定的。

  USB1.1标准接口传输速率为12Mbps,但是一个USB设备最多只可以得到6Mbps的传输频宽。因此若要外接光驱,至多能接六倍速光驱,无法再高。而若要即时播放MPEG-1的VCD影片,至少要1.5Mbps的传输频宽,这点USB办得到,但是要完成数据量大四倍的MPEG-2的DVD影片播放,USB可能就很吃力了,若再加上AC-3音频数据,USB设备就很难实现即时播放了。

  一个USB接口理论上可以支持127个装置,但是目前还无法达到这个数字。其实,对于一台计算机,所接的周边外设很少有超过10个的,因此这个数字是足够我们使用的。

  USB还有一个显著优点就是支持热插拔,也就是说在开机的情况下,你也可以安全地连接或断开USB设备,达到真正的即插即用。 不过,并非所有的Windows系统都支持USB。目前,Windows系统中有许多不同的版本,在这些版本中,只有Windows98以上版本的系统对USB的支持较好,而其他的Windows版本并不能完整支持USB。例如Windows95的零售版是不支持USB的,只有后来与PC捆绑销售的Windows95版本才支持USB。

  目前USB设备虽已被广泛应用,比较普遍的是USB2.0接口,它的传输速度为480Mbps每秒。用户的需求,是促进科技发展的动力,厂商也同样认识到了这个瓶颈。这时, COMPAQ、Hewlett Packard、Intel、Lucent、Microsoft、NEC和PHILIPS这7家厂商联合制定了USB 2.0接口标准。USB 2.0将设备之间的数据传输速度增加到了480Mbps,比USB 1.1标准快40倍左右,速度的提高对于用户的最大好处就是意味着用户可以使用到更高效的外部设备,而且具有多种速度的周边设备都可以被连接到USB 2.0的线路上,而且无需担心数据传输时发生瓶颈效应。

  所以,如果你用USB 2.0的扫描仪,就完全不同了,扫一张4M的图片只需0.1秒钟左右的时间,一眨眼就过去了,效率大大提高。

  而且,USB2.0可以使用原来USB定义中同样规格的电缆,接头的规格也完全相同,在高速的前提下一样保持了USB 1.1的优秀特色,并且,USB 2.0的设备不会和USB 1.X设备在共同使用的时候发生任何冲突。

  USB2.0兼容USB1.1,也就是说USB1.1设备可以和USB2.0设备通用,但是这时USB2.0设备只能工作在全速状态下(12Mbit/s)。USB2.0有高速、全速和低速三种工作速度,高速是480Mbit/s,全速是12Mbit/s,低速是1.5Mbit/s。其中全速和低速是为兼容USB1.1和USB1.0而设计的,因此选购USB产品时不能只听商家宣传USB2.0,还要搞清楚是高速、全速还是低速设备。USB总线是一种单向总线,主控制器在PC机上,USB设备不能主动与PC机通信。为解决USB设备互通信问题,有关厂商又开发了USB OTG标准,允许嵌入式系统通过USB接口互相通信,从而甩掉了PC机。

  新USB2.0规范重新命名了USB标准将原先的USB 1.1改成了USB 2.0 Full Speed(全速版),同时将原有的USB 2.0改成了USB 2.0High-Speed(高速版),并同时公布了新的标识。不言而喻,高速版的USB 2.0速度当然超过全速版的USB 2.0。

  电脑USB端口可以提供最大电流为500mA。