Connector Technology & Design
  • Technologies
  • More
Connector Technology & Design
Forum Does Anyone Have a Project that Could Use Wago's Pluggable Tools-Free Connectors?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • More
  • Cancel
  • New
Join Connector Technology & Design to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 39 replies
  • Subscribers 124 subscribers
  • Views 8264 views
  • Users 0 members are here
Related

Does Anyone Have a Project that Could Use Wago's Pluggable Tools-Free Connectors?

rscasny
rscasny over 3 years ago

imageI was speaking with WAGO who would like to some element14 members to use some of its pluggable connectors.

We first discussed a roadtest. In general, we don't roadtest connectors unless they are part of a larger eval kit. The timing for a design challenge for the remainder of this year isn't quite right as far as scheduling goes.

So, we thought we would ask if any of you would need their products for a project you are doing? If so, we would get some for you.

Let me tell you about the Wago pluggable connectors:

WAGO's pluggable connection system provides a 'tools free' solution for your wiring applications. The system includes seven product lines (2.5–7.62 mm/0.98–0.3 inch pin spacing) and terminates conductors ranging from 0.08 to 10 mm2 (28–8 AWG), offering a wide range of application possibilities.

imageFeatures:

  • Versatile pluggable connection system for continuous system wiring
  • Easy cable pre-assembly and on-unit wiring via vertical and horizontal actuation for the CAGE CLAMP® variants
  • Push-in CAGE CLAMP® termination of both solid and ferruled conductors
  • 100% protection against mismating that's easy to implement
  • Compact and versatile designs
  • Easy-to-customize coding options
  • Intuitive and tool-free lever actuation
  • Universal connection for all conductor types
  • Push-in termination of solid and ferruled conductors
  • Test slot 90° to conductor entry
  • 100% protected against mismating
  • Coding option available
  • Rapid in-the-field connections

Resource Links:

Mfr Page

Rapid Field Connections

If any of you have a project and would like to get some of these connectors, please leave a comment below. 

  • Sign in to reply
  • Cancel

Top Replies

  • scottiebabe
    scottiebabe over 3 years ago in reply to anniel747 +5
    Not to be confused with the
  • beacon_dave
    beacon_dave over 3 years ago +4
    scottiebabe 'Scottiebabe Deluxe Edition' PST widget ? /technologies/test-and-measurement/b/blog/posts/pst-program-the-pico-scpi-labtool?CommentId=202841e3-5717-4d6c-b602-fdb848ffb95c
  • neuromodulator
    neuromodulator over 3 years ago +4
    These look very nice. I'm working on a project where I'll need these kind of connectors at some point (probably next year). The low end screw-based terminal blocks have many inconveniences compared to…
Parents
  • misaz
    misaz over 3 years ago

    I think that connectors are suitable for RoadTest. I understand that for example bare chips are not, but actualy very few vendors provide connector evaluation boards. Picking 10 connectors (differing in pin count, pitch, ...) from the family and giving 2-5pcs each for RoadTest is the best option I think.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • misaz
    misaz over 3 years ago

    I think that connectors are suitable for RoadTest. I understand that for example bare chips are not, but actualy very few vendors provide connector evaluation boards. Picking 10 connectors (differing in pin count, pitch, ...) from the family and giving 2-5pcs each for RoadTest is the best option I think.