Connector Technology & Design
  • Technologies
  • More
Connector Technology & Design
Forum Does Anyone Have a Project that Could Use Wago's Pluggable Tools-Free Connectors?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Connector Technology & Design to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 39 replies
  • Subscribers 125 subscribers
  • Views 8151 views
  • Users 0 members are here
Related

Does Anyone Have a Project that Could Use Wago's Pluggable Tools-Free Connectors?

rscasny
rscasny over 3 years ago

imageI was speaking with WAGO who would like to some element14 members to use some of its pluggable connectors.

We first discussed a roadtest. In general, we don't roadtest connectors unless they are part of a larger eval kit. The timing for a design challenge for the remainder of this year isn't quite right as far as scheduling goes.

So, we thought we would ask if any of you would need their products for a project you are doing? If so, we would get some for you.

Let me tell you about the Wago pluggable connectors:

WAGO's pluggable connection system provides a 'tools free' solution for your wiring applications. The system includes seven product lines (2.5–7.62 mm/0.98–0.3 inch pin spacing) and terminates conductors ranging from 0.08 to 10 mm2 (28–8 AWG), offering a wide range of application possibilities.

imageFeatures:

  • Versatile pluggable connection system for continuous system wiring
  • Easy cable pre-assembly and on-unit wiring via vertical and horizontal actuation for the CAGE CLAMP® variants
  • Push-in CAGE CLAMP® termination of both solid and ferruled conductors
  • 100% protection against mismating that's easy to implement
  • Compact and versatile designs
  • Easy-to-customize coding options
  • Intuitive and tool-free lever actuation
  • Universal connection for all conductor types
  • Push-in termination of solid and ferruled conductors
  • Test slot 90° to conductor entry
  • 100% protected against mismating
  • Coding option available
  • Rapid in-the-field connections

Resource Links:

Mfr Page

Rapid Field Connections

If any of you have a project and would like to get some of these connectors, please leave a comment below. 

  • Sign in to reply
  • Cancel

Top Replies

  • scottiebabe
    scottiebabe over 3 years ago in reply to anniel747 +5
    Not to be confused with the
  • beacon_dave
    beacon_dave over 3 years ago +4
    scottiebabe 'Scottiebabe Deluxe Edition' PST widget ? /technologies/test-and-measurement/b/blog/posts/pst-program-the-pico-scpi-labtool?CommentId=202841e3-5717-4d6c-b602-fdb848ffb95c
  • neuromodulator
    neuromodulator over 3 years ago +4
    These look very nice. I'm working on a project where I'll need these kind of connectors at some point (probably next year). The low end screw-based terminal blocks have many inconveniences compared to…
  • anniel747
    anniel747 over 3 years ago in reply to beacon_dave
    [deleted]
    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago in reply to anniel747

    Not to be confused with the

    image

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to scottiebabe

    Actually, I think that's the tool that they inserted the connector with.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to robogary

    These have lever action. Easier on the fingers than the pushers.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to scottiebabe

    Could perhaps continue on with your Pico carrier type board concept but with jumpered connections to some of those Wago pluggable connectors. These jumpers could be cuttable PCB tracks between pads that allow expansion headers to be soldered in only if you need them. That carrier board gives basic GPIO connectivity to the Pico through the Wago connectors.

    Then if you want to add the likes of the  ADS1115 sampling board functionality you remove the jumpers and drop in a shield/proto board on top of the headers which then reroutes the Pico pins to the shield/proto board and then back to the Wago pluggable connectors, allowing you to add in in whatever additional feature you want.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • kmikemoo
    kmikemoo over 3 years ago in reply to anniel747

    I'm not as enamored with these connectors as I used to be - especially after inserting a four pin one 180 degrees out.  Fortunately, the circuit was able to withstand the mistake.

    For robogary ... me not Neanderthal.  Ug.  Laughing  I was genuinely shocked - and disappointed - by how easily the backward insertion went in.  I use the connector as a training aid these days.

    I would be more forgiving if it was some of the cheap eBay stuff I buy, but this was on a commerical board with name brand connectors.  I like the ribs on the Wago's pictured above.  

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • robogary
    robogary over 3 years ago in reply to kmikemoo

    Me Neanderthal.  Grinning  

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • neuromodulator
    neuromodulator over 3 years ago

    These look very nice. I'm working on a project where I'll need these kind of connectors at some point (probably next year). The low end screw-based terminal blocks have many inconveniences compared to these pluggable lever-based connectors.

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 3 years ago in reply to kmikemoo

    I once managed to plug a 25 pin D  connector into the back of a PC the wrong way round. My excuse is that the location was very hard to access and the connector body was unusually weak (for metal).

    Of course I ended up removing the PC from its nest in a rack and replacing the connector so no time was saved by trying to do it by feel !

    MK

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 3 years ago

    Pretty nice connector line. It would be a good opportunity for me to use my bootlace crimper, although I don't have a suitable project in the works at the moment. For me, getting into a new connector series is about deciding to stock them and use them regularly. I can usually do that just from datasheets, but starting with a small stock is an added incentive. For anyone with a current project this is a great opportunity.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
<>