Connector Technology & Design
  • Technologies
  • More
Connector Technology & Design
Forum Sumimoto Automotive DL series connectors 6098-2156, 8100-2514, 8240-4882, 6098-1626
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • More
  • Cancel
  • New
Join Connector Technology & Design to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 126 subscribers
  • Views 716 views
  • Users 0 members are here
  • connectors
  • sumimoto
Related

Sumimoto Automotive DL series connectors 6098-2156, 8100-2514, 8240-4882, 6098-1626

Stuart_S
Stuart_S over 1 year ago

I've been searching for these parts so I can make a couple of car audio harnesses for a test jig and they seem a bit hard to find.

the part no's are

16P Housing plug 6098-1624, female terminal pin 8240-4882

20P Housing plug 6098-2056 (16 +4) with female terminal pins 8100-2514(16x) and 8240-4882(4x)

They were used some time ago on FMSAudio car radios for Aussie Fords (AU Falcons,Fairmonts -LTDs)  and Nissans about 1998-2002

If anyone has some of these lying about I'd be happy to arrange a trade.

Cheers!

Stuart

  • Sign in to reply
  • Cancel
Parents
  • anniel747
    anniel747 over 1 year ago
    This reply was deleted.
    • Cancel
    • Cancel
Reply
  • anniel747
    anniel747 over 1 year ago
    This reply was deleted.
    • Cancel
    • Cancel
Children
  • Stuart_S
    0 Stuart_S over 1 year ago in reply to anniel747

    Yes, there are female type adapters to fit onto the plug (on vehicle harness ) but I can't find anything male to plug into the radio. I'm looking for the CD adapter type mainly the 6098-1626 which is the 16 pin used plug into the head unit for the CD stacker. I'm building an inline adapter for an AU1 Fairlane as it there is no AUX-IN and I will inject audio via the stacker L+R inputs - it also needs M-Bus data from the stacker to keep it alive. I could simply cut the stacker cable but I'm hoping to make something plug and play so the stacker can remain in situ while it still has a laser left.