Connector Technology & Design
  • Technologies
  • More
Connector Technology & Design
Forum What's the worst contemporary connector you could have on a piece of hardware?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • More
  • Cancel
  • New
Join Connector Technology & Design to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 27 replies
  • Subscribers 129 subscribers
  • Views 689 views
  • Users 0 members are here
  • connectors
  • USB 3.0 Micro B
  • Micro-HDMI
  • communication
Related

What's the worst contemporary connector you could have on a piece of hardware?

OwainM
OwainM 1 month ago

Hey everyone,

A small thought experiment came to mind today when discussing what the worst or most inconvenient connector or connector combination you could find on a device is? I'm specifically thinking of obscure or compact variants of common connector standards.

It came to mind when discussing a Sony camera I have which includes Micro-HDMI Output, or the USB 3.0 Micro B port Samsung used on one of their phones a few years ago.


What is the worst still contemporary connector you could find yourself using is?

If you can't think of anything, what is the most inconvenient connector type you once used, that was contemporary at the time?

I'm intrigued to hear what you've had to use, or at least commiserate together Sweat smile.

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw 1 month ago +5
    It is really annoying when companies like Apple use a standard connector but use a different pinout from the standard.
  • balajivan1995
    balajivan1995 1 month ago +4
    Micro-B, and I mean the high-speed version that's only used on SATA HDD/SSD enclosures. I've never seen it used anywhere else, and it usually just come bundled with the enclosure as a free accessory. One…
  • shabaz
    shabaz 1 month ago +3
    SCART : ) Extremely useful, you wouldn't want a TV without it at the time, but impossible to plug in without perfect alignment* (and orientation precise to a degree or so!) - not possible with the back…
Parents
  • ralphjy
    ralphjy 1 month ago

    In my old age with poor eyesight and arthritic hands, I find that the smaller connectors are the worst problem - always have been to some extent.  The worst is the u.FL connector that is used to connect parts on PCBs to external antenna cables.  It is a pain to connect and disconnect those, especially if the PCB designer doesn't provide enough clearance to other components to enable use of a tool.  It is a miracle, but I've never damaged one of those yet.  My other issue is with some of the flat ribbon cable PCB connectors like those that are used to connect cameras and displays (CSI, DSI).  The plastic piece that is used to clamp the cable end is very fragile.  And I have broken a few of those.

    My other peeve that is not related to connector design but to standards is the 2mm JST connectors that are on small Lithium battery cables.  The RC toy/model standard and the one used by vendors like Adafruit have the + and - connections reversed and not many boards are protected against incorrect polarity.  I am very careful and have never damaged anything, but I have many of both styles of batteries and mating cables/connectors.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • ralphjy
    ralphjy 1 month ago

    In my old age with poor eyesight and arthritic hands, I find that the smaller connectors are the worst problem - always have been to some extent.  The worst is the u.FL connector that is used to connect parts on PCBs to external antenna cables.  It is a pain to connect and disconnect those, especially if the PCB designer doesn't provide enough clearance to other components to enable use of a tool.  It is a miracle, but I've never damaged one of those yet.  My other issue is with some of the flat ribbon cable PCB connectors like those that are used to connect cameras and displays (CSI, DSI).  The plastic piece that is used to clamp the cable end is very fragile.  And I have broken a few of those.

    My other peeve that is not related to connector design but to standards is the 2mm JST connectors that are on small Lithium battery cables.  The RC toy/model standard and the one used by vendors like Adafruit have the + and - connections reversed and not many boards are protected against incorrect polarity.  I am very careful and have never damaged anything, but I have many of both styles of batteries and mating cables/connectors.

    • Cancel
    • Vote Up +3 Vote Down