Connector Technology & Design
  • Technologies
  • More
Connector Technology & Design
Forum What's the worst contemporary connector you could have on a piece of hardware?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • More
  • Cancel
  • New
Join Connector Technology & Design to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 27 replies
  • Subscribers 129 subscribers
  • Views 689 views
  • Users 0 members are here
  • connectors
  • USB 3.0 Micro B
  • Micro-HDMI
  • communication
Related

What's the worst contemporary connector you could have on a piece of hardware?

OwainM
OwainM 1 month ago

Hey everyone,

A small thought experiment came to mind today when discussing what the worst or most inconvenient connector or connector combination you could find on a device is? I'm specifically thinking of obscure or compact variants of common connector standards.

It came to mind when discussing a Sony camera I have which includes Micro-HDMI Output, or the USB 3.0 Micro B port Samsung used on one of their phones a few years ago.


What is the worst still contemporary connector you could find yourself using is?

If you can't think of anything, what is the most inconvenient connector type you once used, that was contemporary at the time?

I'm intrigued to hear what you've had to use, or at least commiserate together Sweat smile.

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw 1 month ago +5
    It is really annoying when companies like Apple use a standard connector but use a different pinout from the standard.
  • balajivan1995
    balajivan1995 1 month ago +4
    Micro-B, and I mean the high-speed version that's only used on SATA HDD/SSD enclosures. I've never seen it used anywhere else, and it usually just come bundled with the enclosure as a free accessory. One…
  • shabaz
    shabaz 1 month ago +3
    SCART : ) Extremely useful, you wouldn't want a TV without it at the time, but impossible to plug in without perfect alignment* (and orientation precise to a degree or so!) - not possible with the back…
Parents
  • shabaz
    shabaz 1 month ago

    SCART : ) Extremely useful, you wouldn't want a TV without it at the time, but impossible to plug in without perfect alignment* (and orientation precise to a degree or so!) - not possible with the back of the TV against the wall.

    * I believe in connector world the technical term is "gatherability", i.e. how much the connectors can be misaligned and still be able to connect. SCART gatherability was not great.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • dang74
    dang74 1 month ago in reply to shabaz

    Just curious, do newer TVs for the European market still have SCART?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dang74
    dang74 1 month ago in reply to shabaz

    Just curious, do newer TVs for the European market still have SCART?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Jan Cumps
    Jan Cumps 1 month ago in reply to dang74

    My last one - a 5 year old smart TV - doesn't. The previous one still had one..

    Also, no more SCART on the recent cable decoder that I got from the provider. Previous version had it.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • OwainM
    OwainM 1 month ago in reply to Jan Cumps

    My 5-year old TV doesn't feature SCART either, and an RCA to Four-pole 3.5mm jack is needed for an RCA Connection

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave 1 month ago in reply to dang74

    Looks like France mandated it to be present on TVs from around 1980 to 2015.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz 1 month ago in reply to OwainM

    A lot of RCA connectors are quite bad because they get used in the wrong environment : ( in-car hi-fi. After a while, poor connection and crackly sound appears : ( One or two mnfr make really nice RCA connectors though; Pomona from memory, their outer connection doesn't loosen as easily.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave 1 month ago in reply to shabaz

    A lot don't have an outer connection to start with... bzzzzzz....

    Also ground tends to mate after signal.