Connector Technology & Design
  • Technologies
  • More
Connector Technology & Design
Polls Poll: How Significant is Single Pair Ethernet Technology to Engineers and the Industry?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • More
  • Cancel
  • New
Join Connector Technology & Design to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: rscasny
  • Date Created: 16 May 2020 1:39 AM Date Created
  • Last Updated Last Updated: 11 Oct 2021 2:59 PM
  • Views 2165 views
  • Likes 2 likes
  • Comments 5 comments
Related
Recommended

Poll: How Significant is Single Pair Ethernet Technology to Engineers and the Industry?

Ethernet has been the go-to communication and network protocol in LAN applications for decades It enables the seamless data transmission via TCP/IP. But Ethernet is evolving from the 4- and 8-wire cabling systems to simpler two-wire cabling, called Single Pair Ethernet technology.

 

Poll Question: How Significant is Single Pair Ethernet Technology to engineers and the industry?

  • community survey
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • mp2100
    mp2100 over 6 years ago +2
    I‘m looking forward to seeing this get rolled out. For a lot of uses, the SPE at 10 Mbps is ’good enough’. I don’t need Gbps for everything. I like the idea of the 1000 meter range of it, for use in sensor…
  • DAB
    DAB over 6 years ago +1
    Ethernet was always expected to expand beyond the initial implementation both for more complex and more simple connections. The initial design envisioned tapping into small computers at low data rates…
  • frostybeard
    frostybeard over 6 years ago +1
    In automotive, this is the only kind of ethernet you find - the two-wire twisted pair. They want things to be light and robust in cars. The connectors are not the standard ethernet connectors, but something…
Parents
  • DAB
    DAB over 6 years ago

    Ethernet was always expected to expand beyond the initial implementation both for more complex and more simple connections.

     

    The initial design envisioned tapping into small computers at low data rates to huge complexes of multiple lines to achieve high bandwidth.

     

    We are just seeing the standard being implemented as intended.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 6 years ago

    Ethernet was always expected to expand beyond the initial implementation both for more complex and more simple connections.

     

    The initial design envisioned tapping into small computers at low data rates to huge complexes of multiple lines to achieve high bandwidth.

     

    We are just seeing the standard being implemented as intended.

     

    DAB