Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Blog CMake: a MACRO can simplify your Pico build
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 27 Aug 2024 12:45 PM Date Created
  • Views 2081 views
  • Likes 11 likes
  • Comments 15 comments
  • raspberry
  • pico
  • cmake
  • vscode
  • teseo_c++
Related
Recommended

CMake: a MACRO can simplify your Pico build

Jan Cumps
Jan Cumps
27 Aug 2024

The Pico C/C++ SDK, and its examples, make extensive use of CMake. If you develop projects that use the same principles, you 'll be familiar with the CMake configuration file  CMakeList.txt.

A simple project, that builds a single firmware and relies on the SDK API only, will have a straightforward CMake config file. If your project builds more than one deliverable, the file can get big. You may end up with (almost identical) repeating sections. In that case, a macro can help to keep this manageable. And to maintain integrity of the build when making changes later.

My project C++ library for ST Teseo GPS builds 3 different firmware binaries, and each of them has a UART and I2C version. I used a macro to keep the CMake configuration doable

A CMake macro is very similar to the C parameterised macro. During the project configuration, each declaration that uses the macro, will be expanded. The values used will replace the macro parameters.

Here is my firmware build macro:

# macro to build firmware binary for the examples
macro(__build_firmware example protocol)
message("building firmware for example ${example}, protocol ${protocol}")

add_executable(${CMAKE_PROJECT_NAME}_${example}_${protocol}
        ${CMAKE_CURRENT_SOURCE_DIR}/teseo_${example}.cpp
        ${CMAKE_CURRENT_SOURCE_DIR}/gps_nmea_lib/nmea/nmea.cpp       
)

target_link_libraries(${CMAKE_PROJECT_NAME}_${example}_${protocol} 
        ${CMAKE_PROJECT_NAME}_shared_${protocol}
)

target_include_directories(${CMAKE_PROJECT_NAME}_${example}_${protocol} PUBLIC 
${CMAKE_CURRENT_SOURCE_DIR}/gps_nmea_lib/nmea
)

# select the debug output (optional, not used by the GPS interface)
pico_enable_stdio_uart(${CMAKE_PROJECT_NAME}_${example}_${protocol} 1)
pico_enable_stdio_usb(${CMAKE_PROJECT_NAME}_${example}_${protocol} 0)

pico_add_extra_outputs(${CMAKE_PROJECT_NAME}_${example}_${protocol} )

endmacro()

The parameters are example and protocol.

Here is the code to build one of the 3 firmware binaries, for both their UART and I2C variant:

# build teseo reply response example --------------------------------------

__build_firmware("reply_response" "uart")

__build_firmware("reply_response" "i2c")

I repeated this for each of the examples. The outcome is that a build all nicely creates all binaries:

building firmware for example reply_response, protocol uart
building firmware for example reply_response, protocol i2c
building firmware for example with_nmea_parse, protocol uart
building firmware for example with_nmea_parse, protocol i2c
building firmware for example nmea_with_data_processing, protocol uart
building firmware for example nmea_with_data_processing, protocol i2c
-rw-r--r-- 1 runner docker 161280 Aug 26 16:31 build/pico_gps_teseo_reply_response_uart.uf2
-rw-r--r-- 1 runner docker 161280 Aug 26 16:31 build/pico_gps_teseo_reply_response_i2c.uf2
-rw-r--r-- 1 runner docker 198144 Aug 26 16:31 build/pico_gps_teseo_with_nmea_parse_uart.uf2
-rw-r--r-- 1 runner docker 198144 Aug 26 16:31 build/pico_gps_teseo_with_nmea_parse_i2c.uf2
-rw-r--r-- 1 runner docker 195584 Aug 26 16:32 build/pico_gps_teseo_nmea_with_data_processing_uart.uf2
-rw-r--r-- 1 runner docker 195584 Aug 26 16:32 build/pico_gps_teseo_nmea_with_data_processing_i2c.uf2

This is one example of how macros can help. Further reading: https://cmake.org/cmake/help/latest/command/macro.html.

Link to all posts.

  • Sign in to reply
Parents
  • scottiebabe
    scottiebabe over 2 years ago

    A riscv blinky.

    image

    This is the cmake list vscode generated

    # Generated Cmake Pico project file
    
    cmake_minimum_required(VERSION 3.13)
    
    set(CMAKE_C_STANDARD 11)
    set(CMAKE_CXX_STANDARD 17)
    set(CMAKE_EXPORT_COMPILE_COMMANDS ON)
    
    # Initialise pico_sdk from installed location
    # (note this can come from environment, CMake cache etc)
    
    # == DO NEVER EDIT THE NEXT LINES for Raspberry Pi Pico VS Code Extension to work ==
    if(WIN32)
        set(USERHOME $ENV{USERPROFILE})
    else()
        set(USERHOME $ENV{HOME})
    endif()
    set(sdkVersion 2.0.0)
    set(toolchainVersion RISCV_COREV_MAY_24)
    set(picotoolVersion 2.0.0)
    include(${USERHOME}/.pico-sdk/cmake/pico-vscode.cmake)
    # ====================================================================================
    set(PICO_BOARD pico2 CACHE STRING "Board type")
    
    # Pull in Raspberry Pi Pico SDK (must be before project)
    include(pico_sdk_import.cmake)
    
    project(blink C CXX ASM)
    
    # Initialise the Raspberry Pi Pico SDK
    pico_sdk_init()
    
    # Add executable. Default name is the project name, version 0.1
    
    add_executable(blink
        blink.c
        )
    
    # pull in common dependencies
    target_link_libraries(blink pico_stdlib)
    
    if (PICO_CYW43_SUPPORTED)
        target_link_libraries(blink pico_cyw43_arch_none)
    endif()
    
    # create map/bin/hex file etc.
    pico_add_extra_outputs(blink)
    
    # add url via pico_set_program_url
    

    appears similar to other pico projects except

    set(toolchainVersion RISCV_COREV_MAY_24)
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to scottiebabe

    You generated it via that VSCode plug-in, he?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • scottiebabe
    scottiebabe over 2 years ago in reply to scottiebabe

    Wild. Even the debug probe sort of works with riscv

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to scottiebabe

    I'm installing it...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • scottiebabe
    scottiebabe over 2 years ago in reply to Jan Cumps

    I was getting throtled when VSCode tried to DL https://buildbot.embecosm.com/job/corev-gcc-win64/50/artifact/corev-openhw-gcc-win64-20240602.zip 

    Plus the vscode downloader/installer can't tolerate a network connection change it just gives up and deletes the partial download.

    So I downloaded/unziped it separately.

    The RISCV toolchain is 7 GB when extracted

    image

    The DL zip file is 1.8 GB.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to scottiebabe

    I'm still in ARM land. Haven't bought a Pico 2 yet ...

    I'm procrastinating, until FreeRTOS releases an SMP port for the RISCV pair

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to scottiebabe

    The plugin works, with my XIAO based PicoProbe in CDAP mode:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to scottiebabe

    The plugin works, with my XIAO based PicoProbe in CDAP mode:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • scottiebabe
    scottiebabe over 2 years ago in reply to Jan Cumps

    Congrats!

    The out of box experience for baremetal c/c++ is night and day from when they released the first pico...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to scottiebabe

    Maybe we can create a plugin discussion post, after some experimentation.

    2 initial thoughts:

    • easy to get started. Easy to get a project that will build and can be debugged. This was quite a challenge in the past.
    • not that VSCode look-and-feel savvy. Not evident how to select a different toolchain. The standard VSCode way is not available in a plugin created project. No setting in the plugin to change it ... 
      Good news is that it uses GCC 13_2_Rel1
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • scottiebabe
    scottiebabe over 2 years ago in reply to Jan Cumps

    Yes its not as easy to switch in an existing project

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to scottiebabe

    Do you use a nightly release? I don't see that option.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • scottiebabe
    scottiebabe over 2 years ago in reply to Jan Cumps

    Do you have a show/hide button

    image

    On windows I have v0.15.2

    image

    I just used the version listed in vs code available extensions which turns out to be the latest

    https://github.com/raspberrypi/pico-vscode 

    On a PI4 I can't get the VSiX to install...