Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Blog EasyL1105: A Dev Board for the TI ARM Cortex-M0+ L-Series
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 10 Aug 2025 11:07 PM Date Created
  • Views 4430 views
  • Likes 11 likes
  • Comments 70 comments
  • MSPM0L1105
  • MSPM0
  • arm cortex
  • cortex-m0+
  • easyL1105
  • arm cortex-m
  • texas instruments
  • MSPM0L1106
  • ti
Related
Recommended

EasyL1105: A Dev Board for the TI ARM Cortex-M0+ L-Series

shabaz
shabaz
10 Aug 2025

Table of Contents

  • Introduction
  • Circuit Description
    • 1. Microcontroller Core
    • 2. USB UART
    • 3. Voltage Regulator
  • Circuit Board
  • Building and Running an Example Project
  • Summary

 

TLDR Section

The easyL1105 is a TI MSPM0L1105 Development Board that can be DIY'd. Here are the links:

Schematic PDF

PCB Gerber Zip file

Parts List PDF

For more blogs and information: Use the searchbox, tags are easyL1105 or MSPM0

easyL1105 GitHub repository page

Introduction

I was browsing the Texas Instruments (TI) website, and noticed they had some very low-cost, very basic ARM Cortex-M0+ microcontrollers. I was keen on finding something low-power, small (but hand-solderable), and cheap. I aim to eventually use such a chip for interfacing to simple sensors for a few possible projects (one requires some sort of low-accuracy current sensor, and another requires an presence sensor), so all I require is a basic built-in ADC, I2C, SPI, or perhaps UART, and either control an output, or send text to an I2C LCD display, or perhaps write to external SPI storage.

In the end, I decided to order a few parts from the TI MSPM0 L-Series, which they class as low-power, and I found a 28-pin variant which has a fair amount of general-purpose input/output (GPIO) connections.

The microcontroller doesn’t have any particularly remarkable features, other than the very low power consumption and cheapness, and the fact that it doesn’t require many components at all, not even a crystal oscillator. Just a few decoupling capacitors are all that’s technically required.

image

(Image source: Microcontroller PDF Datasheet)

In shutdown (with GPIO wakeup capability), current consumption is apparently 61 nA, which seems pretty low. RAM can be maintained and timers can be running in a ‘standby’ mode, where current consumption is 1uA, which also seems reasonable.

One more thing I really liked; it has an in-built bootloader that can accept firmware over the serial (UART) port, so that no separate programmer device is required for in-the-field updates. You could just attach it directly to a PC and program it up.

The particular part I went for is the L1105 (the full name is MSPM0L1105TDGS28R), which has 32 kByte of Flash memory and 4 kByte of RAM, but there is a pin-compatible L1106 upgrade part with 64 kByte of Flash if needed.

In terms of major downsides, there’s no ability to add a crystal oscillator if you need such precision. Interestingly, as a compromise, the chip can use an external 0.1% tolerance 100k resistor in order to create a reasonably precise internal oscillator, but it won’t compare with a crystal, of course. I would have liked an accurate RTC, but I suppose that could always be an external I2C peripheral chip, perhaps with a separate backup battery.

TI doesn’t actually have a dev-board for this particular L1105 part, but since it’s a simple chip, I’d much rather make my own dev-board, so I can get used to working with the chip without all the extras that many dev-boards have.

Circuit Description

The circuit is split up into three main sections, described next. For the PDF version of the schematic and the project files, see the easyL1105 project repository on GitHub.

1. Microcontroller Core

The core of the circuit is shown below (click to enlarge).

This doesn’t do much, other than breaking out most of the microcontroller connections to 0.1” pin headers. I took a reasonable guess at how the pins might be used, and so some are labelled with I2C and SPI connection names. A couple of pins are useful for timer-based input/output capabilities; for instance, one could use them for attaching a rotary encoder. As a simple user interface, the circuit has a single button (SW3) and a couple of LEDs attached to GPIO pins; it’s up to the user to write code to make use of that button and the LEDs.

There is a 5-pin header, J5, that can be used to attach a traditional SWD JTAG programmer device if required.

The BSL_RX and BSL_TX connections are used for uploading firmware via serial. To enable this, there is a BSL_BOOT button that needs to be held down during a reset. There are some non-populated resistor pads attached to the BSL_BOOT switch, because I’m unsure if that pin floats, or if the user may wish to permanently set that to a particular level.

image

Note: It was later discovered that this Rev 1 circuit is missing a 47k pull-up resistor, from the *RST pin (pin 6 on the microcontroller) to +3.3V. It was easy to patch onto the underside of the PCB.

image

2. USB UART

Since I was keen to use the serial bootloader, the dev-board contains a USB-UART adapter. It’s based around a CH340K USB-UART chip, which I’ve never used before. The chip is a little unusual in that it uses pull-up resistors on the UART side if the chip is powered from 5V and not from the (lower) microcontroller voltage; that’s the reason for R16 on the right side of the circuit (R18 is not fitted, otherwise the microcontroller will always start in bootloader mode!). After some discussion with Jan Cumps  it's likely R16 is not needed, so it could potentially be removed (depending on if the RX pin is floating or not on the microcontroller). The microcontroller reset pin is wired through a jumper on J3 to the RTS line, in case it is possible to automatically reset the board from the PC (if you're using the official TI app, UniFlash, then it's not possible, and the jumper needs to be removed). You would still need to manually press the BSL_BOOT button (although, if the microcontroller is new from the factory with the Flash erased, then for that first time the BSL_BOOT button doesn’t need to be pressed).

The pin headers labelled J3 are used with shorting jumpers to redirect the USB-UART from the BSL pins to alternative pins for UART0. This is so that the same USB-UART can be used for general program serial input/output, too.

image

3. Voltage Regulator

The final bit of circuitry is a 3.3V regulator, which can be powered either by the USB connection or from a 5V labelled connection that is exposed on the GPIO pin headers. The two shorting jumpers can be used to separate the power to the microcontroller portion of the circuitry from the rest of the board. By removing the shorting jumpers, you could wire in a separate power supply if desired, or attach current measurement circuitry.

image

Circuit Board

An approximate render of the circuit board is shown below; it is about 60 x 40 mm.

image

Underside:

image

Building and Running an Example Project

All the steps are described at the README file in the easyL1105 GitHub repository. Scroll down to the Example Project section to see the detail. By following the steps there, it is possible to build using either Keil or with GCC. The Keil steps were tested with Windows. GCC was tested with Windows and Linux.

The steps to use TI's UniFlash tool, for uploading the built .hex firmware file to the board, are also described at the same location.

Summary

TI’s MSPM0 L-series microcontrollers offer low-power and low-cost, and a simple development board was created for the 28-pin L1105 part (32 kByte Flash and 4 kByte RAM). The dev-board brings out most of the connections on the microcontroller, and also allows the testing of the serial bootloader capability of the chip, so that it can be programmed in the field, by connecting to a PC without any programmer hardware required.

The KiCad files and PCB files for sending to any PCB manufacturer are in the EasyL1105 GitHub repository. Although the board has not been tested yet (Edit: it has now been assembled and tried out. See the comments below for information about how to use the board). If you give it a go, it would be interesting to hear any feedback.

Also, if you have any ideas/uses for such a board or a similar one, it would be great to hear about them.

Thanks for reading.

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 1 year ago +1
    Maybe worth mentioning how I'm soldering this. Apologies for the low-quality photos, they were taken with mobile phone. I used a small bent-conical tip, but it's not that critical. First step, apply…
  • shabaz
    shabaz 4 months ago +1
    Finally upgraded the PCBs for EasyL1105 and miniL1105, to revision 2.0! Gerber files are here . The EasyL1105 board is now a tiny bit longer, because the components were squashed up otherwise. This board…
  • shabaz
    shabaz 1 month ago in reply to shabaz +1
    So close, yet so far! I messed this up. This is the faulty circuit: I made a semi-fix by moving *RST to pin 11 of U3. It is still not great, but works to an extent. With this semi-fix, the bootloader…
  • shabaz
    shabaz 4 months ago

    Couldn't resist another change, this would be revision 2.1, if I go ahead with it.

    It replaces the UART0/BSL switching jumpers with a FET switching array. A small tweak in the MSPM0 Python programmer software can then make *DTR go low (and stay low) for the entire programming cycle, hence routing the BSL_RX/TX pins to the USB-UART. It would mean zero fiddling with jumper pins when programming the device. The only downside is that you'd have to use the Python programmer with the EasyL1105 board, because I'm sure the official programmer (TI UniFlash) won't control the *DTR pin like this. It seems a small disadvantage, because I cannot see myself ever wanting to use UniFlash for this microcontroller, when the Python programmer is so much quicker to use.

    I've tested that setting *DTR low (and setting the BOOT Invoke pin high) during the entire programming cycle seems to work, so hopefully this is a low-risk modification (if I've got the switch array wiring right! If anyone spots any mistakes, please let me know. I'll lay out these changes onto the PCB sometime this weekend. 

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz 4 months ago

    Finally upgraded the PCBs for EasyL1105 and miniL1105, to revision 2.0! Gerber files are here.

    The EasyL1105 board is now a tiny bit longer, because the components were squashed up otherwise. This board fixes the Rev 1.0 clash between the BSL Invoke pin, and UART0. Circuit diagram here and also the issue with higher-than-desired voltage from the USB-UART chip. It also included auto-boot and auto-reset, so that (if desired) no buttons need to be held down to program the Flash; it's controlled by the PC software automatically.

    image

    This is the Rev 2.0 miniL1105 board, which is DIP-24 sized (schematic) and requires an external programmer (SWD-based, or USB UART):

    image

    These are untested, but I've ordered them and will test them at some point.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz 5 months ago in reply to Jan Cumps

    Looking forward to your discoveries with it! The extra GPIO and additional peripherals (also two I2C and two UARTs I think) will come in very handy for projects.

    If it goes well for you, I'll order some of the ICs in my next order to try too. I like how simple it was to use the L1105 hence this 1306 sounds attractive.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps 5 months ago

    I ordered a Launchpad for another child in the MSPM0L family: the 1306. It has more peripherals, but still part of that low energy group.

    image

    The package isn't as hand-solder friendly as the VSSOP used here in the EasyL1105 design. But still doable. 

    Comparison:


    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps 11 months ago

    I'm porting and investigating TI's GUI example

    image

    This example uses TI's "JSON GUI" on the EasyL1105, and their standard GUI Demo running in my laptop browser. Comms is over UART.

    Everything is interrupt driven on the MSPM0. When you change the controls on the right, the GUI sends a JSON payload.
    On the MSPM0, a UART RX interrupt fires. The JSON GUI functions then investigate the payload, and call your matching callback.
    If you slide the boolean to enable, the gauge gets updated by the amount set in the slider., every timer tick (also an interrupt)

    When you press a button on the EasyL1105, a GUI interrupt fires, and increments one of the counters. That data is sent over UART. The graph values are updates (orange / red lines)

    Each timer interrupt, 2 things happen:

    - a counter gets updated (the blue line in the graph)

    - the current data set is sent over UART (and the browser GUI updates itself when it receives that data)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>