Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Blog Engineering THE WALKING DEAD - the perpetual motion generator
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 12 Dec 2016 3:01 AM Date Created
  • Views 3460 views
  • Likes 1 like
  • Comments 12 comments
  • zombies
  • zombie power
  • alternative energy
  • engineering the walking dead
  • diy
  • Design
  • cabeatwell
  • power grid
  • etwd
  • twd
  • the walking dead
  • power
Related
Recommended

Engineering THE WALKING DEAD - the perpetual motion generator

Catwell
Catwell
12 Dec 2016

CLICK THIS INFORGRAPHIC IMAGE BELOW!

image

http://twitter.com/Cabe_Atwell

  • Sign in to reply

Top Comments

  • Catwell
    Catwell over 9 years ago in reply to hnrbnd +2
    Jay Watson, I don't believe that zombies from The Walking Dead universe were found or shown to eat for energy. Their systems were reactivated by the virus. They stop moving only when they are completely…
  • mcb1
    mcb1 over 9 years ago +1
    Interesting idea. I thought that zombies migrate to humans in order to convert them into zombies. If that is the case you'd need something at the end that the zombie thought was a human, ie more than 1…
  • spannerspencer
    spannerspencer over 9 years ago in reply to mcb1 +1
    Yeah, like a carrot and stick kind of set up, to keep the zombies in motion. The movie practically writes itself.
Parents
  • michaelkellett
    michaelkellett over 9 years ago

    In your "calculations" you fail to consider the reaction force on the Zombie.

     

    Lets get this into sensible units:

    4kW of output, 54 inches/second on the treadmill belt = 1.4m/s

    the force required to move the belt will be 4000/1.4 = 2857 N

    assume the Zombie weighs 75kg, then you'll need a coefficient of friction between the Zombie's foot and the treadmill of 3.8 - which is not credible without teeth on the belt which would be cruel.

     

    Worse, in all the films the Zombies are about human equivalent in power and strength and humans can't manage more than 100W or so for long periods - if Zombies can do 40x better they'll have us on the treadmills.

     

    AND - you haven't allowed for losses in the treadmill, generator etc.

     

    This isn't going to work.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • michaelkellett
    michaelkellett over 9 years ago

    In your "calculations" you fail to consider the reaction force on the Zombie.

     

    Lets get this into sensible units:

    4kW of output, 54 inches/second on the treadmill belt = 1.4m/s

    the force required to move the belt will be 4000/1.4 = 2857 N

    assume the Zombie weighs 75kg, then you'll need a coefficient of friction between the Zombie's foot and the treadmill of 3.8 - which is not credible without teeth on the belt which would be cruel.

     

    Worse, in all the films the Zombies are about human equivalent in power and strength and humans can't manage more than 100W or so for long periods - if Zombies can do 40x better they'll have us on the treadmills.

     

    AND - you haven't allowed for losses in the treadmill, generator etc.

     

    This isn't going to work.

     

    MK