Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Blog Free graphics display designer tool for PICs
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: MicrochipRTCfr
  • Date Created: 26 Jun 2010 9:46 AM Date Created
  • Views 1463 views
  • Likes 0 likes
  • Comments 4 comments
  • oled
  • pic24
  • tft
  • frame_buffer
  • pic24f256da210
  • lcd_controller
  • qvga
  • vga
  • pic32
Related
Recommended

Free graphics display designer tool for PICs

MicrochipRTCfr
MicrochipRTCfr
26 Jun 2010

Looking for faster & free embedded GUI design ?

 

The Graphics Display Designer tool enables graphical design of the user interface and generates C code which can be directly compiled into libray calls using the free Microchip compilers.

Code can then be tested using the Graphics development kits based on PIC24F/H, dsPIC33 or PIC32 processors.

For highest integration, PIC24F family with on-chip graphics LCD controller can be used and developed with the new PIC24FJ256DA210 Development Kit

  • Sign in to reply
  • MicrochipRTCfr
    MicrochipRTCfr over 15 years ago

    Hi,

     

    I suggest you open a ticket on Microchip support website 

    You may also get help from the Microchip community graphics forum or compiler forum here : http://forum.microchip.com

     

    regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    Question about the Graphics Display Designer V2.0.1.9 (with updated Library):
    Is there a limit to the number of type="picture" elements (widgets) that can be added to a screen? I have 18 and get errors when running Code Generation: "GDD Files Not Present..." The files are present, since I just use a total of 17 pictures and all works fine. I am trying to come up with work-arounds but nothing appears to work. Interestingly, if I add more than 18 images, numerous errors result and subsequent Exit of GDD crashes MPLAB with a memory fault. (Sounds like someone is mismanaging an array somewhere.)

    Any help would be great!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • MicrochipRTCfr
    MicrochipRTCfr over 15 years ago in reply to e14 Contributor

    Hi,

     

    You should not confuse the chip capabilities and the graphics libraries specification.

    As far as the PIC24FJ256DA210 microcontroller is concerned, the specification clearly states :

    "Resolution up to 640x480 @30Hz, 16 bpp, or 480x272 @60Hz, 16 bpp"
    So VGA is achievable but with @30Hz / 16bpp because the controller is at the limit of its throughput.
     
    Even though there is no project example yet in the graphics libraries using VGA, they are not limited in resolution.
    In fact I believe that a Pictail plus board with a VGA display is in preparation and should be available in 2011 from Microchip.
    There is a dedicated forum for graphics libraries questions here.
     
    The external memory is not SDRAM but standard SRAM. You can find the schematics of the graphics display board in the graphics demoboard user manual
     
    regards
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    Dear Sir or Madam,

     

    I'am new in Microchip graphic library and I have one  question. If I would use a PIC24FJ256DA210, according to the datasheet  it is possible to achieve a resolution of 640x480 with 16bpp. This ist  only achievable with further external SDRAM.

     

    I have read in the description of the graphic library that:

    "The Microchip graphics library supports the following features:

    Up to 480x272 (WQVGA) resolution
    Up to 16-bit or 65K colors"

     

    Is  that the limitions of the graphic library (480x272) or is it possible  to design a window with a larger resolution like 640x480 or 800x480?

    I read in chat room that a larger resolution should be possible. It's a little confused!

     

    best regards

    Benjamin Hütter