Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Blog Free graphics display designer tool for PICs
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: MicrochipRTCfr
  • Date Created: 26 Jun 2010 9:46 AM Date Created
  • Views 1464 views
  • Likes 0 likes
  • Comments 4 comments
  • oled
  • pic24
  • tft
  • frame_buffer
  • pic24f256da210
  • lcd_controller
  • qvga
  • vga
  • pic32
Related
Recommended

Free graphics display designer tool for PICs

MicrochipRTCfr
MicrochipRTCfr
26 Jun 2010

Looking for faster & free embedded GUI design ?

 

The Graphics Display Designer tool enables graphical design of the user interface and generates C code which can be directly compiled into libray calls using the free Microchip compilers.

Code can then be tested using the Graphics development kits based on PIC24F/H, dsPIC33 or PIC32 processors.

For highest integration, PIC24F family with on-chip graphics LCD controller can be used and developed with the new PIC24FJ256DA210 Development Kit

  • Sign in to reply
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    Question about the Graphics Display Designer V2.0.1.9 (with updated Library):
    Is there a limit to the number of type="picture" elements (widgets) that can be added to a screen? I have 18 and get errors when running Code Generation: "GDD Files Not Present..." The files are present, since I just use a total of 17 pictures and all works fine. I am trying to come up with work-arounds but nothing appears to work. Interestingly, if I add more than 18 images, numerous errors result and subsequent Exit of GDD crashes MPLAB with a memory fault. (Sounds like someone is mismanaging an array somewhere.)

    Any help would be great!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • e14 Contributor
    e14 Contributor over 15 years ago

    Question about the Graphics Display Designer V2.0.1.9 (with updated Library):
    Is there a limit to the number of type="picture" elements (widgets) that can be added to a screen? I have 18 and get errors when running Code Generation: "GDD Files Not Present..." The files are present, since I just use a total of 17 pictures and all works fine. I am trying to come up with work-arounds but nothing appears to work. Interestingly, if I add more than 18 images, numerous errors result and subsequent Exit of GDD crashes MPLAB with a memory fault. (Sounds like someone is mismanaging an array somewhere.)

    Any help would be great!