Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Blog Getting Started with the USRP B205mini-i software defined radio platform
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: alexwonglik1
  • Date Created: 23 Feb 2021 10:27 PM Date Created
  • Views 5376 views
  • Likes 7 likes
  • Comments 4 comments
  • dft
  • spartan- 6
  • signal
  • python
  • uhf
  • usrp b205mini-i
  • spectrum
  • time domain
  • xilinx
  • transceiver
  • digital signal processing
  • fpga
  • digilent blog
  • frequency domain
  • radio
  • gnu
  • digilent
  • fourier
  • analog devices
  • software defined radio
  • dsp
  • sdr
  • fft
  • labview
  • rf
  • usrp
  • radio frequency
  • frequency
Related
Recommended

Getting Started with the USRP B205mini-i software defined radio platform

alexwonglik1
alexwonglik1
23 Feb 2021

image

 

The USRP B205mini-iUSRP B205mini-i is a flexible and compact platform that is ideal for both hobbyist and OEM applications. It is designed by Ettus ResearchTm and provides a wide frequency range (70 MHz to 6 GHz) and a user-programmable, industrial-grade Xilinx Spartan-6 XC6SLX150 FPGA. The RF front end uses the Analog Devices AD9364 RFIC transceiver with 56 MHz of instantaneous bandwidth. The board is bus-powered by a high-speed USB 3.0 connection for streaming data to the host computer. The USRP B205mini-i also includes connectors for GPIO, JTAG, and synchronization with a 10 MHz clock reference or PPS time reference input signal.

 

The getting started guide walks you through the steps you need to take in order to use the USRP B205mini-i.USRP B205mini-i. You will learn how to install the software driver and GNU radio in Windows or Ubuntu, connect the devices, run examples and create an FM radio receiver from scratch. When you start using the device, there are some examples that come with the driver. You can run the real-time Discrete Fourier Transform (DFT) example. The options for the executable (./rx_ascii_art_dft) are frequency (–freq), sampling rate (–rate), gain (–gain), bandwidth (–bw), and reference level (–ref-lvl). The terminal will show the flow of execution, list the parameters, and graph the result:

 

image

 

Project Example - Using GNU Radio to Design a Frequency Modulation (FM) Receiver

The FM receiver takes the modulated signal (i.e. radio waves under the VHF band) as input and produces the original audio signal ranging from 20 Hz to 20 kHz.

First of all, in the terminal, the GNU Radio Companion will be open. Then, the following blocks will be added: Sample Rate, Frequency, USRP and QT GUI Sink. Next, a low pass filter is used.

Notice that the audio signal bandwidth ranges from 200 Hz to 20 kHz. Once the lowpass filter has been added, the next step is to perform the FM demodulation.

 

image

 

Since the output signal is audible, this signal is sent to the sound card - which is actually a digital to analog converter with a sample rate of, in general, 96 kHz. A Rational resamples block is used, to perform an x/y operation, where x (interpolation) is the output frequency, and y (decimation), is the input frequency. Finally, Audio sink block is added, so that the output signal will be played through speakers. After being generated, the python script is sent to USRP B205mini-i and executed. The output signal is displayed in the time and frequency domain, as seen below.

 

image

image

 

 

Find the complete getting started guide and project examples on the Digilent Reference Page.

  • Sign in to reply

Top Comments

  • nathandumont
    nathandumont over 5 years ago in reply to 14rhb +2
    Only just seen this article via Twitter. I'm just wrapping up my roadtest review for this board so more on it soon. To answer the three points you raised: 1. GNURadio flow-graphs actually generate Python…
Parents
  • 14rhb
    14rhb over 5 years ago

    Hi alexwonglik1

     

    A good introduction, thank you.

     

    There's several posts on E14 currently discussing SDR and perhaps you could answer some questions I have pondered for sometime and been unable to answer from the internet.

    • Once a GNURadio schematic is created and run, where is the majority of that processing undertaken - on the SDR's FPGA or on the host PC ?
    • If not answered in that last question, what purpose does the FPGA play?
    • If processing is undertaken on the host PC, is it possible to wrap that design, and download to the FPGA, such that it is a stand alone RF system without a host PC?
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • alexwonglik1
    alexwonglik1 over 5 years ago in reply to 14rhb
    • I assume you are asking about signal processing. For the USRP B205 mini, that will be on the FPGA device.
    • This page may give you some idea about FPGA role in SDR: https://kb.ettus.com/RFNoC
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • alexwonglik1
    alexwonglik1 over 5 years ago in reply to 14rhb
    • I assume you are asking about signal processing. For the USRP B205 mini, that will be on the FPGA device.
    • This page may give you some idea about FPGA role in SDR: https://kb.ettus.com/RFNoC