Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Blog Lenovo Introduces Snapdragon Chips to its Mini Desktop PCs
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 17 Jan 2025 8:23 PM Date Created
  • Views 2740 views
  • Likes 5 likes
  • Comments 2 comments
  • microsoft
  • ces2025
  • embedded
  • cabeatwell
  • windows
  • ces
  • os
  • arm
  • innovation
Related
Recommended

Lenovo Introduces Snapdragon Chips to its Mini Desktop PCs

Catwell
Catwell
17 Jan 2025

image

Lenovo’s ThinkCentre neo 50q mini desktop is ideal for small and medium businesses and can use up to 16GB of RAM. (Image Credit: Lenovo)

Will this translate to other ARM based platforms? Recently, Qualcomm revealed plans to join the mini desktop world. At CES 2025, Lenovo revealed two of its mini PCs, the ThinkCentre Neo 50q and IdeaCentre Mini X. These will feature Qualcomm’s Snapdragon X series chips, offering Copilot Plus PC functionality. Starting at $659.99, Lenovo’s IdeaCentre Mini X will be available this April. Meanwhile, the ThinkCentre neo 50q QC has a $849 selling price and will be available in February.

image
The IdeaCentre Mini x PC can use either the Snapdragon X chip or the Snapdragon X Plus. (Image Credit: Lenovo)

Lenovo’s IdeaCentre Mini x PC can handle productivity tasks without producing noise and is ideal for those in the creative field. At the front, it comes with a power button, a headphone jack, a USB-A 3.2 Gen 2 port, and a USB-C 3.2 Gen 2 port. Meanwhile, the back includes two USB-A 3.2 Gen 2 ports, a USB-A 2.0 port, a USB-C 4 port, an HDMI 2.1 port, a DisplayPort 1.4 connection, and an Ethernet port. The IdeaCentre Mini x  PC features a built-in power supply and two fans to cool the system. Owners can also easily switch out parts as the unit has an easy-to-open case.

The system uses a base Snapdragon X chip or the Snapdragon X Plus and has up to 1TB of storage and up to 32GB of RAM. This mini-computer also has Wi-Fi 7 connectivity.

image

The ThinkCentre neo 50q is available this February. (Image Credit: Lenovo)

Meanwhile, small and medium businesses can use the ThinkCentre neo 50q. This machine has similar features, including the chip---either Qualcomm’s Snapdragon or the X Plus. However, only 16GB of RAM can be integrated. The front of this system features one USB-A 3.2 Gen 2 port, one USB-C 3.2 Gen 2 port, a power button, and a headphone jack. In the back, it has two USB-A 3.2 Gen 2 ports, two USB-A 2.0 ports, an HDMI 2.1 port, an Ethernet port, and a DisplayPort 1.4 connection. The ThinkCentre neo 50q has Wi-Fi6E connectivity.   

Have a story tip? Message me at: http://twitter.com/Cabe_Atwell

  • Sign in to reply
Parents
  • ariajames_121
    ariajames_121 over 1 year ago

    It is exciting to see Lenovo integrating Snapdragon chips into their mini desktop PCs The move towards ARM-based computing is definitely gaining momentum and it will be interesting to see how these devices perform in terms of efficiency and power consumption Have you had a chance to test one yet or seen any benchmarks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • ariajames_121
    ariajames_121 over 1 year ago

    It is exciting to see Lenovo integrating Snapdragon chips into their mini desktop PCs The move towards ARM-based computing is definitely gaining momentum and it will be interesting to see how these devices perform in terms of efficiency and power consumption Have you had a chance to test one yet or seen any benchmarks.