Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Blog Monarch Go Starter Kit: access to all UARTs
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 25 Jul 2021 2:30 PM Date Created
  • Views 2220 views
  • Likes 6 likes
  • Comments 4 comments
  • monarch
Related
Recommended

Monarch Go Starter Kit: access to all UARTs

Jan Cumps
Jan Cumps
25 Jul 2021

I've reviewed the Monarch Go LTE/4G modem for a road test. For that exercise, the modem was mounted on an Arduino-style shield. And there was a complete software example.

In this post, I am checking the lower levels of the modem. How to directly talk to it and get logging info out.

image

Most of the Monarch Go documentation is available under NDA only. I'm restricting the info here on what's available in public, or what you can find out without the NDA restricted info, by poking at the serial ports of the Starter KIT. and following the traces of the Arduino and Starter KIT PCBs.

 

Four UARTs

When you plug the board in your PC, you'll see that it enumerates 4 ports.

Each of them will have a function. By looking at the behaviour and examples, I could determine the function and settings of the first 2.

The Monarch is 1.8V. If you use the Arduino shield, be careful.

The UART that's connected to the Arduino headers (below called AT UART) has a 1.8 - 3.3 V translator. The other ones aren't 3.3V savvy.

The Starter KIT PCB seems

 

AT UART:

This is the 2nd COM port that enumerates when you plug in the Starter KIT.

It is also used in the example program of the road test.

From the source code, we know it's 115200, 8, N with RTS/CTS.

You can use this one to send AT commands. I started by typing all the commands used in the example code:

 

image

 

console UART:

This one you can find the settings from easily, because there is traffic on it by default.

You can put an oscilloscope or logic analyser on the Arduino shield and figure out the settings.

It's 155200, 8, N, no control.

This port shows what's happening inside the modem.

It also has an interpreter, but I haven't been able to get much out of it.

 

image

 

I found out about the interpreter on that port by connecting putty to it and pressing enter.

image

This is as far as I got with this at the moment.

 

UARTs enumerated as 3 and 4

These don't seem to do a lot. I can connect to those, but I see nothing happening. No reaction when I type, no data coming back.

Info is available under NDA. But that means I can't blog about it.

 

References on element14:

Monarch Go Arduino Shield Adapter Schematic

AES-SQN-MNRCHGO-SHLD1-G Hardware User Guide

AES-SQN-MNRCHGO-HT1-G-HW-UG-V1_0.pdf

Networking with Sequans Monarch Go - Part I (interesting article. With housing measures, also available here)

Sequans Monarch-Go Python Example  (for definition of the 4 enumerated ports, and interesting examples on MQTT and other client protocols available on board of the modem)

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 5 years ago in reply to fmilburn +1
    All info needed to use the modem is publicly available. When you want to use it out of context - in my case out of the certified conditions - you may need more info. I also prefer that all in is the open…
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to fmilburn +1
    I've added useful documentation at the end of the post.
  • Jan Cumps
    Jan Cumps over 4 years ago

    I'm revisiting the exercise.
    In the road test, I followed Avnet's and Sequans' how-to, and used an Azure application that was predefined.
    This time I'd like to try my own solution.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to fmilburn

    I've added useful documentation at the end of the post.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to fmilburn

    All info needed to use the modem is publicly available.

    When you want to use it out of context - in my case out of the certified conditions - you may need more info.

    I also prefer that all in is the open. But I had my coffee image.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 5 years ago

    Most of the Monarch Go documentation is available under NDA only.


    This just seems strange for a product in a RoadTest. There could be a reason, and it might be a good one, but it is more irritating than interesting to read that there are UARTs with capabilities that can’t be disclosed due to the NDA.  It is morning and I just had my coffee. Should be over my grumpiness soon.