Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Blog Renesas Solution Starter Kit for RX23E-A: register configuration for the Thermocouple app note
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 23 Jun 2023 1:21 PM Date Created
  • Views 1456 views
  • Likes 6 likes
  • Comments 7 comments
  • RoadTest
  • RX23e-a
  • d2a28d6e-11d8-11ee-be56-0242ac120002
Related
Recommended

Renesas Solution Starter Kit for RX23E-A: register configuration for the Thermocouple app note

Jan Cumps
Jan Cumps
23 Jun 2023

The kit for Road test: Renesas Solution Starter Kit for RX23E-A comes with a Thermocouple. You work with it via a PC application. By default, that application, and the oob firmware, are set up to directly test the delta sigma ADC. But to test the thermocouple and its cold junction compensation circuit, you need to change the registers. That can be done via the PC Tool, using the Registers tab. I've found the settings in the Thermocouple appnote. Then I configured the registers to reflect that.

image

On the SIM4 tab:

image

Some bits that are set in the thermocouple firmware, I can't seem to set from the PC Tools:

image

I've attached the configuration file. To take care that all registers are set as in the appnote's firmware, I loaded the firmware to the board, ran the app in the PC Tool, then saved all registration settings. That's the file attached to this post.
When loading it to the PC Tool, youy have to load the file twice. The DAC1 reference buffers don't set to enabled after the first load. You need to load the same file again to make it happen. Maybe the order of the register settings?

Example result: bottom trace is ADC1, the PT100, top trace the thermocoupleimage

PC Tool config file: thermocouple_appnote_firmware_register_read_bis.3ea.zip

link to all posts

  • Sign in to reply
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to Jan Cumps

    comparison with my config: 

    left: my PC Tool setup, right the Thermocouple firmware

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago

    Here is the same view, loaded from the RX23e-a running the Renesas' thermocouple firmware. Looks close.
    image
    I haven't reviewed every setting yet...

    Raw register values:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<