Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Blog Self-repairing processor
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Eavesdropper
  • Date Created: 21 Mar 2011 6:10 PM Date Created
  • Views 746 views
  • Likes 1 like
  • Comments 3 comments
  • research
  • microchip
  • chip
  • on_campus
  • repair
  • embedded
  • diagnostic
  • microcontroller
  • university
  • innovation
Related
Recommended

Self-repairing processor

Eavesdropper
Eavesdropper
21 Mar 2011
image
 
CRISP has developed a multi-core processor that will test and repair itself, sort of. There is an on-board resource manager that will test to see if a core is malfunctioning, and if so, send the tasks to a functioning core. The idea is to create a chip that will always work 100% of the time regardless of internal component failures. ‘‘Because of the rapidly growing transistor density on chips, it has become a real challenge to ensure high system dependability. The solution is not to make non-degradable chips, it's to make architectures that can degrade while they keep functioning, which we call graceful degradation. With the right dependability infrastructure many-cores can be a solution', says Hans Kerkhoff accociate professor at the University of Twente.

 
Still in the design, prototype, stage, this technology may very well be the standard future of chip design. My old critic is what is the "resource manager" gets corrupted due to a bad core? I'm sure more details will emerge over time on how they will handle such events.

 
CRISP stands for Cutting edge Reconfigurable ICs for Stream Processing. It is a collaborative effort from the University of Twente, Tampere University of Technology, Thales Netherlands, Recore Systems, Atmel, and NXP at the moment.

 
Eavesdropper
  • Sign in to reply
Parents
  • DAB
    DAB over 15 years ago

    There was a lot of work done on this subject by TRW during the 1990's for integrated avionics.  They approached the problem by using one processor to come up as the master, but each processor in turn would have a timed delay to see if the a master had asserted control.  If not, then the next processor that timed out would assume master control and allocate the processors to tasks as needed.  Based on the block diagram, a similar approach would probably work here.

    Thanks,

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 15 years ago

    There was a lot of work done on this subject by TRW during the 1990's for integrated avionics.  They approached the problem by using one processor to come up as the master, but each processor in turn would have a timed delay to see if the a master had asserted control.  If not, then the next processor that timed out would assume master control and allocate the processors to tasks as needed.  Based on the block diagram, a similar approach would probably work here.

    Thanks,

    DAB