Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Blog Tibbo Project System (TPS) from Tibbo Technology: “Take what you need. Leave out what you don’t.”
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dmitry_slepov
  • Date Created: 13 May 2016 11:57 AM Date Created
  • Views 4122 views
  • Likes 4 likes
  • Comments 17 comments
  • Embedded Systems
  • iot
  • industrial iot
Related
Recommended

Tibbo Project System (TPS) from Tibbo Technology: “Take what you need. Leave out what you don’t.”

dmitry_slepov
dmitry_slepov
13 May 2016

image

Tibbo Project System (TPS) is a highly configurable, affordable, and innovative automation platform. It is ideal for home, building, warehouse, and production floor automation projects, as well as data collection, distributed control, industrial computing, and device connectivity applications.

 

Suppliers of traditional “control boxes” (embedded computers, PLCs, remote automation and I/O products, etc.) typically offer a wide variety of models differing in their I/O capabilities. Four serial ports and six relays. Two serial ports and eight relays. One serial port, four relays, and two sensor inputs. These lists go on and on, yet never seem to contain just the right mix of I/O functions you are looking for.

 

Rather than offering a large number of models, Tibbo Technology takes a different approach: Our Tibbo Project System (TPS) utilizes TibbitsRegistered – miniature electronic blocks that implement specific I/O functions. Need three RS232 ports? Plug in exactly three RS232 Tibbits! Need two relays? Use a relay Tibbit. This module-based approach saves you money by allowing you to precisely define the features you want in your automation controller.

Here is a closer look at the process of building a custom Tibbo Project System.

 

 

Start with a Tibbo Project PCB (TPP)

 

image

 

A Tibbo Project PCB is the foundation of TPS devices.

Available in two sizes – medium and large – each board carries a CPU, memory, an Ethernet port, power input for +5V regulated power, and a number of sockets for Tibbit Modules and Connectors.

 

Add TibbitRegistered Blocks

image

 

Tibbits (as in “Tibbo Bits”) are blocks of prepackaged I/O functionality housed in brightly colored rectangular shells. Tibbits are subdivided into Modules and Connectors.

Want an ADC? There is a Tibbit Module for this. 24V power supply? Got that! RS232/422/485 port? We have this, and many other Modules, too.

Same goes for Tibbit Connectors. DB9 Tibbit? Check. Terminal block? Check. Infrared receiver/transmitter? Got it. Temperature, humidity, and pressure sensors? On the list of available Tibbits, too.

 

 

Assemble into a Tibbo Project Box (TPB)

image

 

Most projects require an enclosure. Designing one is a tough job. Making it beautiful is even tougher, and may also be prohibitively expensive. Finding or making the right housing is a perennial obstacle to completing low-volume and hobbyist projects.

Strangely, suppliers of popular platforms such as Arduino, Raspberry Pi, and BeagleBone do not bother with providing any enclosures, and available third-party offerings are primitive and flimsy.

Tibbo understands enclosure struggles and here is our solution: Your Tibbo Project System can optionally be ordered with a Tibbo Project Box (TPB) kit.

The ingenious feature of the TPB is that its top and bottom walls are formed by Tibbit Connectors. This eliminates a huge problem of any low-volume production operation – the necessity to drill holes and openings in an off-the-shelf enclosure.

The result is a neat, professionally looking housing every time, even for projects with the production quantity of one.

Like boards, our enclosures are available in two sizes – medium and large. Medium-size project boxes can be ordered in the LCD/keypad version, thus allowing you to design solutions incorporating a user interface.

 

 

Unique Online Configurator

 

 

To simplify the process of planning your TPS we have created an Online Configurator.

Configurator allows you to select the Tibbo Project Board (TPP), “insert” Tibbit Modules and Connectors into the board’s sockets, and specify additional options. These include choosing whether or not you wish to add a Tibbo Project Box (TPB) enclosure, LCD and keypad, DIN rail mounting kit, and so on. You can choose to have your system shipped fully assembled or as a parts kit.

Configurator makes sure you specify a valid system by watching out for errors. For example, it verifies that the total power consumption of your future TPS device does not exceed available power budget. Configurator also checks the placement of Tibbits, ensuring that there are no mistakes in their arrangement.

Completed configurations can be immediately ordered from our online store. You can opt to keep each configuration private, share it with other registered users, or make it public for everyone to see.

 

 

Develop your application

image



Like all programmable Tibbo hardware, Tibbo Project System devices are powered by Tibbo OS (TiOS).

Use our free Tibbo IDE (TIDE) software to create and debug sophisticated automation applications in Tibbo BASIC, Tibbo C, or a combination of the two languages.

To learn more about the Tibbo Project System please visit http://tibbo.com/tps.html. TPS parts, as well as complete systems can be ordered from our online store (http://tibbo.com/store/tps.html).

  • Sign in to reply

Top Comments

  • michaelkellett
    michaelkellett over 10 years ago in reply to dougw +1
    I can't see much point - as an example I looked at the Tibbit Block 13, you pay $27 for a $5 LTC2309 and in return you can only access 4 of the 8 analogue inputs on the chip. You'll need an additional…
  • dmitry_slepov
    dmitry_slepov over 10 years ago in reply to dougw +1
    Mr. Douglas, Our new boards coming out now are using ST32 ARM micros.
  • dmitry_slepov
    dmitry_slepov over 10 years ago in reply to balearicdynamics +1
    Enrico, thank you for taking your time to write this detailed comment. There is one part I really do not understand -- the part about the soldering and using just once. Tibbits PLUG into our mainboards…
Parents
  • dougw
    dougw over 10 years ago

    Very interesting concept. I like the great modularity.

    What are the specifications for the T1000 CPU?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 10 years ago in reply to dougw

    I can't see much point - as an example I looked at the Tibbit Block 13, you pay $27 for a $5 LTC2309 and in return you can only access 4 of the 8 analogue inputs on the chip. You'll need an additional block to get terminals and you still have to solder it to the board. You don't get any input protection, buffering etc so in most applications you'll need additional of board hardware (and  a pcb to put it on).

     

    For my money you're way better off with a simple dev board (ST Nucleo or other manufacturers' equivalents) - much cheaper, much more open about what parts are used and their specs.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dmitry_slepov
    dmitry_slepov over 10 years ago in reply to michaelkellett

    Mr. Michael,

     

    It is not true that Tibbit #13 is "just a single IC". This Tibbit DOES have input protection, as well as noise filtering on its power lines. The block diagram shown on our website is just that -- a simplified block diagram.The TPS value proposition comes to these two things: - you don't have to solder anything, and - you automatically have a very nice housing. The second part is extremely important. Yes, there are many "flexible" and inexpensive boards on the market, but they all lack the enclosure. Without the enclosure, your creation will always look like something temporary, designed only to be tested in the lab, and not suitable to be deployed in the real world. With TPS, we are trying to be halfway between bare boards like Raspberry Pi and REALLY expensive products like WAGO I/O controllers. Compared to WAGO, our prices are pretty decent! So, that's how we position ourselves: high-end hobbyist market to "modestly" professional market.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 10 years ago in reply to dmitry_slepov

    If you don't put the full spec on your website where it can easily be found you can't expect people to guess what's inside the little boxes. 

     

    And if you don't know what's inside you can't readily work out if they are suitable for your application. The cheapo development boards all have full published schematics - if you match that it improves your proposition quite a bit.

     

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dmitry_slepov
    dmitry_slepov over 10 years ago in reply to michaelkellett

    Mr. Michael

     

    Kindly visit our website: tibbo.com

     

    Here you can find all information regarding Tibbits: Shop TibbitRegistered Blocks — Tibbo Technology

     

    Thank you!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 10 years ago in reply to dmitry_slepov

    I looked at your website before I made any comment at all:

     

    no specs, no proper technical documentation, no schematics.

     

    If I'm wrong, then please link on your website to schematic off Tibbit #13, max sample rate of same, any details of speed, latency etc etc.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dmitry_slepov
    dmitry_slepov over 10 years ago in reply to michaelkellett

    Mr. Kellett,

     

    my apologies. OK, it is true that we have a lot a lot of documenting to do. At the same time, our documentation is not that non-existent. Look at the manuials:

     

    The hardware: Tibbo Document System

    The software, programming, etc: TIDE, TiOS, Tibbo BASIC and Tibbo C Manual

     

    Regarding the specs for the Tibbit #13, I do realize that we need to do more work on this. Because the Tibbit is based on a particular ADC, we felt it wasn't necessary to copy the entire spec from this IC's datasheet. Some things are just inherited. Still, there are some things that should go into the documentation. I fully agree with you on this. We will improve.

     

    We are also going to publish the schematics of our Tibbit modules.

     

    Best Regards,

    Dmitry

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dmitry_slepov
    dmitry_slepov over 10 years ago in reply to michaelkellett

    Mr. Kellett,

     

    my apologies. OK, it is true that we have a lot a lot of documenting to do. At the same time, our documentation is not that non-existent. Look at the manuials:

     

    The hardware: Tibbo Document System

    The software, programming, etc: TIDE, TiOS, Tibbo BASIC and Tibbo C Manual

     

    Regarding the specs for the Tibbit #13, I do realize that we need to do more work on this. Because the Tibbit is based on a particular ADC, we felt it wasn't necessary to copy the entire spec from this IC's datasheet. Some things are just inherited. Still, there are some things that should go into the documentation. I fully agree with you on this. We will improve.

     

    We are also going to publish the schematics of our Tibbit modules.

     

    Best Regards,

    Dmitry