Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Analogue Design 9V NiMH charging
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 14 replies
  • Subscribers 526 subscribers
  • Views 4000 views
  • Users 0 members are here
  • charging
  • nimh
  • battery
Related

9V NiMH charging

koudelad
koudelad over 2 years ago

Hello,

9V batteries have always been a pain for me... Expensive, low capacity, almost every DMM / tester needed them.

I just bought a 9V NiMH battery: https://www.westinghousebattery.com/Ni-MH-Rechargeable/Premium-Series.html . To my surprise, it is not made from 6 smaller cells (which would give ca. 7.2-8.4 V), but 7, which has nominal voltage of 8.4, but when charged, can have almost 10 V. This makes it a true primary 9V battery replacement. I am not sure when these became available, but I remember older 6-cell "9 V" NiMH that were kind of useless, because all appliances thought the battery is discharged, due to the lower nominal voltage.

However, I never really had a charger for this kind of battery. I have heard that cheap chargers only use 12 V DC power supply with in series resistor in series to limit the current to ca 30 mA.

Do you have any suggestion for a charging circuit? I am open to building something, even using an MCU. I would love it to have a small small charging current (20-30 mA) or slightly higher (50 mA), a safety timer and the delta V detection. There is a famous old MAX713 charger, but according to the features, it offers C/4 to 4C charging and C/16 trickle charging, which is too high. Most commercially available hobby chargers also have a minimum current of 100 mA.

Thank you,

David

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 2 years ago in reply to shabaz +5
    I had some time, to lay out the PCB. This board is 100 x 60 mm and several different PP3 battery holders will fit. All parts are jellybean. The optional microcontroller is connected to the row of pin-headers…
  • shabaz
    shabaz over 2 years ago +3
    I think the circuit below would do it. It's based off of a simpler charger here: Smart Doorbell System – Part 6 – Chime Module Complete Circuit Design and based on information from a battery mnfr PDF doc…
  • genebren
    genebren over 2 years ago in reply to shabaz +3
    Very Nice! This is something that I would like to look into further in the future. I really do appreciate your efforts to assist and to promote a true sense of community here on element14!
Parents
  • scottiebabe
    0 scottiebabe over 2 years ago

    I use a USB-C PD module, diode, resistor, and ohms law FTW.

    If you want to make your own PCB you could consider an switching LED driver and design around a 5V USB input.

    One random example:

    image

    ww1.microchip.com/.../mic2287c.pdf

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 2 years ago in reply to scottiebabe

    Cool idea, but I'm wondering if it would tend to try to overcharge, as it tries to maintain a constant current?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dougw
    0 dougw over 2 years ago in reply to scottiebabe

    Cool idea, but I'm wondering if it would tend to try to overcharge, as it tries to maintain a constant current?