Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
DSP Forum 450MHz Shark DSP Dev-kits
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 171 subscribers
  • Views 2835 views
  • Users 0 members are here
  • fram
  • mhz
  • lcd
  • sdram
  • tft
  • mandelbrot
  • spi
  • uart
  • dsp
  • dev
  • sram
  • analog
  • shark
  • kits
Related

450MHz Shark DSP Dev-kits

Kilohercas
Kilohercas over 12 years ago

Hello, does any one are interested in Analog devices Shark development kit ?

 

image

 


Basically it is ADSP-21489 floating point DSP running at 450MHz ( possible to 700MHz overclock) with all pins connected to header (except single UART for debugging and boot pins for spi flash since i am using dual channel FT2232 for debugging/programing)

 

I made Labview program that can program external SPI flash with FT2232D  from Labview by using loader file generated inside  Crosscore or VisualDSP++ IDE. This can be very high performance calculation engine for demanding applications. I can do single point DFT with 128 array at 2MHz repetition rate, while ARM Cortex M4 (STM32F407 running 250MHz can only do 50KHz !! )

 

Here is what Shark DSP can do in native calculation image (Mandelbrot fractal in f32 )

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

At the moment i have single unpopulated board , but can order more if demand is big. With additional cost i can buy all parts, assemble and ship it as full development kit.

  • Sign in to reply
  • Cancel
Parents
  • mikewolak
    mikewolak over 12 years ago

    Hi Linas,

     

    I'd be interested in one of these boards, unpopulated or otherwise. Does it also have a JTAG programming header? I can be reached at mikewolak @ gmail . com .

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Kilohercas
    Kilohercas over 12 years ago in reply to mikewolak

    Since i don't have jtag for analog products (USB_ICE) and it cost more than i can spend , programming is done by using FTDI FT2232D SPI interface.

     

    Idea is simple: hold DSP in reset, so all pins are in high-z state, enable bus drivers connected to FT2232D SPI output ( same pin as hold DSP in reset), delete flash ( as many pages as needed for ldr file) and when all data is inside flash, disable bus drivers to high-z state and release DSP from reset.

     

    imageimage

    Only problem i am facing right now is that i need to hold reset button while i programming DSP, even when i probe it, FT2232 does hold DSP in reset without any problems. Small problem, i guess i need to add some delay inside programming loop for bus drivers since if i enable them with reset button and when release, flash is programmed correctly

     

    skype kilohercas
    gmail>> megahercas6@.....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Kilohercas
    Kilohercas over 12 years ago in reply to mikewolak

    Since i don't have jtag for analog products (USB_ICE) and it cost more than i can spend , programming is done by using FTDI FT2232D SPI interface.

     

    Idea is simple: hold DSP in reset, so all pins are in high-z state, enable bus drivers connected to FT2232D SPI output ( same pin as hold DSP in reset), delete flash ( as many pages as needed for ldr file) and when all data is inside flash, disable bus drivers to high-z state and release DSP from reset.

     

    imageimage

    Only problem i am facing right now is that i need to hold reset button while i programming DSP, even when i probe it, FT2232 does hold DSP in reset without any problems. Small problem, i guess i need to add some delay inside programming loop for bus drivers since if i enable them with reset button and when release, flash is programmed correctly

     

    skype kilohercas
    gmail>> megahercas6@.....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to Kilohercas

    Very interesting ! i'm looking for something like this to begin programing, dsp guitar effects