Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
DSP Forum 450MHz Shark DSP Dev-kits
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 171 subscribers
  • Views 2829 views
  • Users 0 members are here
  • fram
  • mhz
  • lcd
  • sdram
  • tft
  • mandelbrot
  • spi
  • uart
  • dsp
  • dev
  • sram
  • analog
  • shark
  • kits
Related

450MHz Shark DSP Dev-kits

Kilohercas
Kilohercas over 12 years ago

Hello, does any one are interested in Analog devices Shark development kit ?

 

image

 


Basically it is ADSP-21489 floating point DSP running at 450MHz ( possible to 700MHz overclock) with all pins connected to header (except single UART for debugging and boot pins for spi flash since i am using dual channel FT2232 for debugging/programing)

 

I made Labview program that can program external SPI flash with FT2232D  from Labview by using loader file generated inside  Crosscore or VisualDSP++ IDE. This can be very high performance calculation engine for demanding applications. I can do single point DFT with 128 array at 2MHz repetition rate, while ARM Cortex M4 (STM32F407 running 250MHz can only do 50KHz !! )

 

Here is what Shark DSP can do in native calculation image (Mandelbrot fractal in f32 )

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

At the moment i have single unpopulated board , but can order more if demand is big. With additional cost i can buy all parts, assemble and ship it as full development kit.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 11 years ago

    Hello.

    Do you still have Sharc development boards for sale?

     

    thank you?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Kilohercas
    Kilohercas over 11 years ago in reply to e14 Contributor

    Yes

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to Kilohercas

    If you prefer to talk in private my email is ealfie _at_ gmail _dot_ com

     

    do you have a datasheet, manual or something like that?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to Kilohercas

    If you prefer to talk in private my email is ealfie _at_ gmail _dot_ com

     

    do you have a datasheet, manual or something like that?