Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
DSP Forum Algo for rms computation?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 166 subscribers
  • Views 3063 views
  • Users 0 members are here
Related

Algo for rms computation?

ggabe
ggabe over 3 years ago

I’m entertaining a true rms computation on MSPM0G3507 for the 10Hz…100KHz range. 

The MCU is limited to 32K RAM, so I’d change the sampling frequency if I can determine the signal is periodic and in the lower frequency range.

Is there any algorithm that aims capture N periods of a periodic signal? 

Should I be better of by going into frequency domain with a proper window function, and possibly trying multiple sampling rates to choose the proper range?

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 3 years ago +1
    What's wrong with: sample (at 500kHz) s square (at 500kHz) sq = s * s mean (at 500kHz) m = m + ( (sq - m) / Ki) square root (at read out rate) rms = m ^ 0.5 Division by a constant can be done…
  • ggabe
    ggabe over 3 years ago in reply to scottiebabe +1
    Yes, it is interesting. TI is selling the EVB for $16 direct. The part is very much a new item, TI is not sampling it yet. The accelerator is cool, but not as advanced as the MSP430's LEA. The benefit…
  • ggabe
    ggabe over 3 years ago in reply to michaelkellett +1
    I think the algorithm with Ki used to be referred as exponential decay averaging. The alternative, the moving averaging has a sensitivity when the weight of the partial periods start to influence the average…
Parents
  • ggabe
    ggabe over 3 years ago

    After a little digging, I'm to do autocorrelation and finding the peaks. Would autocorrelation be as good use of the CPU resources as FFT?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • ggabe
    ggabe over 3 years ago

    After a little digging, I'm to do autocorrelation and finding the peaks. Would autocorrelation be as good use of the CPU resources as FFT?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • ggabe
    ggabe over 3 years ago in reply to ggabe

    It turns out autocorrelation can be easily calculated by FFT/IFFT, per  Wiener-Khinchin. I’m onto something!