Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Power delivery IC
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 20 replies
  • Subscribers 505 subscribers
  • Views 5109 views
  • Users 0 members are here
Related

Power delivery IC

aster94
aster94 over 6 years ago

Hello,

 

Discalaimer: I am an hobbyst, not a professional

 

I am looking for a IC that change the output from a USB-C from 5v to 12v. I was able to find a few IC (like STUSB4700 from STM but there are others) that can do this, but all the IC i found need to be connected to a master I2C. Since i run out of pins, and i would like an easier solution i would like to have a chip that can change the power delivery from the standard 5v to 12v. On aliexpress i found the IP2721 (see here: https://stackoverflow.com/questions/58666162/type-c-usb-c-trigger-set-lowest-voltage-allowed ) which is perfect for my needs but it has a chinese datasheet and doesn't seem easy t find.

 

Do you know any solution?

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 6 years ago in reply to aster94 +4
    Is this something you could use? USB-C Power Delivery Sink (CYPD3177)
  • aster94
    aster94 over 6 years ago +2
    At the end i bought the module with the IP2721 I am writing here just in case someone finds this topic because today i found the stusb4500 ( https://www.st.com/en/interfaces-and-transceivers/stusb4500…
  • wolfgangfriedrich
    wolfgangfriedrich over 6 years ago in reply to Jan Cumps +2
    Thanks, Jan Cumps . I saw this thread just now.
Parents
  • Jan Cumps
    Jan Cumps over 6 years ago

    The STUSB4700 is an IC for the 'provider side'. It's part of the supply, not a device you use on the consume side to negotiate an output. STUSB1602 is a 'sink side' device.

    On the EEVblog, they are designing a µCurrent supply that uses Type-C PD. They have a hard time.

     

    It's possible to implement in a microcontroller. ST has a software solution for their controllers ...

    I haven't seen single-IC solutions that can get 12 V out of a USB-C connector just with passives. Maybe there's a market for that ...

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • seulater
    seulater over 6 years ago in reply to Jan Cumps

    "On the EEVblog, they are designing a µCurrent supply that uses Type-C PD. They have a hard time."

     

    That does not mean anything The kid they have working there is not a seasoned engineer. He just got out of school, so dont put any faith on what they "can" or "cannot do"

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • seulater
    seulater over 6 years ago in reply to Jan Cumps

    "On the EEVblog, they are designing a µCurrent supply that uses Type-C PD. They have a hard time."

     

    That does not mean anything The kid they have working there is not a seasoned engineer. He just got out of school, so dont put any faith on what they "can" or "cannot do"