Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Power delivery IC
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 20 replies
  • Subscribers 505 subscribers
  • Views 5102 views
  • Users 0 members are here
Related

Power delivery IC

aster94
aster94 over 6 years ago

Hello,

 

Discalaimer: I am an hobbyst, not a professional

 

I am looking for a IC that change the output from a USB-C from 5v to 12v. I was able to find a few IC (like STUSB4700 from STM but there are others) that can do this, but all the IC i found need to be connected to a master I2C. Since i run out of pins, and i would like an easier solution i would like to have a chip that can change the power delivery from the standard 5v to 12v. On aliexpress i found the IP2721 (see here: https://stackoverflow.com/questions/58666162/type-c-usb-c-trigger-set-lowest-voltage-allowed ) which is perfect for my needs but it has a chinese datasheet and doesn't seem easy t find.

 

Do you know any solution?

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 6 years ago in reply to aster94 +4
    Is this something you could use? USB-C Power Delivery Sink (CYPD3177)
  • aster94
    aster94 over 6 years ago +2
    At the end i bought the module with the IP2721 I am writing here just in case someone finds this topic because today i found the stusb4500 ( https://www.st.com/en/interfaces-and-transceivers/stusb4500…
  • wolfgangfriedrich
    wolfgangfriedrich over 6 years ago in reply to Jan Cumps +2
    Thanks, Jan Cumps . I saw this thread just now.
  • seulater
    seulater over 6 years ago in reply to aster94

    The part you are looking for is the FUSB302BMPX

     

    https://www.digikey.com/product-detail/en/on-semiconductor/FUSB302BMPX/FUSB302BMPXCT-ND/6138870

     

    A guy made these boards with one.

    https://www.tindie.com/products/clarahobbs/pd-buddy-sink/?utm_source=Hackaday&utm_medium=Banner&utm_campaign=HAD_Tindie_Banners

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to seulater

    Regarding your comment:

    The part you are looking for is the FUSB302BMPX

    what bit of this requirement:

    USB-C power delivery controller that can be driven only with passive components

    does that part meet? The power delivery is controlled using I2C using the part you refer to.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • seulater
    seulater over 6 years ago in reply to shabaz

    I guess I missed that part in his post. My apologies.

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • phoenixcomm
    phoenixcomm over 6 years ago in reply to aster94

    aster94 unobtainium

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 6 years ago in reply to seulater

    I take exception to your comments to shabaz "Google does not find everything, and should not be the "go-to" place...."

    and to Jan Cumps "That does not mean anything The kid they have working there...." and extend your apology.

     

    Your comments were dismissive, with a touch of arrogance. The E14 Community ranking the two members have, reflects both their experience and knowledge level. It also demonstrates their commitment to this community. I have yet to have them offer a glib reply. Their responses carry some weight in my Rolodex of members that have the answers that I can use and their willingness to share.

     

    Maybe I should cut you some slack as your profile status indicates "Just joined the community."  After being a member for 8 years you might have learned some comment decorum. 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • phoenixcomm
    phoenixcomm over 6 years ago in reply to phoenixcomm

    aster94 sorry for my comment i thought you wanted a "passive" way to do this.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 6 years ago

    GreatScott! (with µC)

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • seulater
    seulater over 6 years ago

    Using the STUSB4500 you can program it with your options and it will save them. So you only need the I2C to program it once.

    Sparkfun has a board for this.

    https://learn.sparkfun.com/tutorials/power-delivery-board---usb-c-qwiic-hookup-guide?_ga=2.154539768.1712984379.15923166…

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • hawk_789
    hawk_789 over 6 years ago

    It took me a while to figure all this out and Im a retired engineer, lol. First you need to decide whether to use an already made board or are going to design your PCB as well. I chose the latter. Evaluation boards will be pricey for the beginner. Being I already had the ATMEL IDE and interface for all their micro controllers, I decided on their chip USB7206. Its a 100 pin QFN and handles all the power profiles up to 20VDC at 5A. Of course you have the power supply to deliver the power to start with. It just has a power rail in the chip.It is about $9.00.

    This chip carries you to a full 10gb  data transfer speed.

     

    If you do not need that speed,  the Arduino was supposed to make one with PD for the USB3.0 The micro controller above is for 3.1 gen 2. The only thing I could find on the Arduino which is called Micro PD was just some crowd funding.

     

    I'm sure that all this is too late for you but perhaps it will help others

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • phoenixcomm
    phoenixcomm over 6 years ago in reply to Jan Cumps

    all I can say is WOW!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<