Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Sensing 5 dB and lower sounds
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 503 subscribers
  • Views 1382 views
  • Users 0 members are here
Related

Sensing 5 dB and lower sounds

aster94
aster94 over 6 years ago

Hello,

 

I would like to built a heart beat sensor (note: no, it is not an ECG) that sense the sound made from the heart (phonocardiography) and converts it in a digital signal.

I am writing here for suggestion about how to achieve it.

I did a little bit of researches and found that a heart beat should be around 10-15dB (source: The Decibel ). Actually an heart beat is made by 4 different sounds so i guess that the article refers to the most audible (S1) so for my application I think that would be good to aim at around 5dB.

 

image

 

I wasn't able to find a dedicated sound sensor (maybe i didn't search enough?), i found a few comparator or amplifier like the lm393 used in these application. Also on google i found the existence of Surface acoustic wave sensors (https://en.wikipedia.org/wiki/Surface_acoustic_wave_sensor) that maybe could suit my needs.

 

What i would like to do has been already done in digital stethoscopes (https://www.worthview.com/stethoscope-amplify-sound/).

 

Do you think that what i would like to do is feasible? how would you do it?

 

Thanks in advance

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 6 years ago in reply to aster94 +3
    These people make good microphones but they are expensive: https://www.gras.dk/microphone-guide/dynamic-range You can see that you need a big diameter to get the performance you need. I don't think that…
  • aster94
    aster94 over 6 years ago in reply to shabaz +2
    I thought that a piezo was something not very good for this, but i shall reconsider this, I just found an interesting table that shows that some of the most important stethoscopes (3M) is actually using…
  • shabaz
    shabaz over 6 years ago +1
    Hi Vincenzo, A piezo disc can be used. There's probably better ways, but as a schoolkid experimenting at the time, I certainly was able to hear heartbeat with just a piezo disc and something like an LM386…
Parents
  • shabaz
    shabaz over 6 years ago

    Hi Vincenzo,

     

    A piezo disc can be used. There's probably better ways, but as a schoolkid experimenting at the time, I certainly was able to hear heartbeat with just a piezo disc and something like an LM386, and headphones. The disc needs a plastic rim, and enclosure (could be 3D-printed).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 6 years ago

    Hi Vincenzo,

     

    A piezo disc can be used. There's probably better ways, but as a schoolkid experimenting at the time, I certainly was able to hear heartbeat with just a piezo disc and something like an LM386, and headphones. The disc needs a plastic rim, and enclosure (could be 3D-printed).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • aster94
    aster94 over 6 years ago in reply to shabaz

    I thought that a piezo was something not very good for this, but i shall reconsider this, I just found an interesting table that shows that some of the most important stethoscopes (3M) is actually using it.

     

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 6 years ago in reply to aster94

    These people make good microphones but they are expensive:

     

    https://www.gras.dk/microphone-guide/dynamic-range

     

    You can see that you need a big diameter to get the performance you need.

     

    I don't think that anyone make piezo microphones any more -  the last one I designed was about 1977 !

    (Not a real new design, re-working a microphone based on a Rochelle salt element to use a ceramic element - sensitivity was way lower with the ceramic.)

     

    I've got no data on it now but here's an ad I found on the web with a picture of the original - the company I worked for made the microphone under license to Cosmocord in the mid to late 1970s.

     

    image

     

    If you can get this type of microphone it might be OK - the source capacity is many times greater than an electret or capacitive element so the LF noise can be lower.

    A moving coil microphone could give low noise if you can find a suitable element.

    Best I could see on Aliexpress were these:

    https://www.aliexpress.com/item/32915426371.html?spm=a2g0o.productlist.0.0.5ea18047Oj3XvL&algo_pvid=4b0e9b7e-e98a-4a31-8…

    (Shure clones - cardioid response so not ideal but 600ohm impedance and high sensitivty can give very low noise.)

     

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • aster94
    aster94 over 6 years ago in reply to michaelkellett

    unfortunately my knowledge in this field is near zero so if you suggest that microphone I am going to buy it, even if I would rather to use something smaller