Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Cyclone II Max Clock Rate
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 497 subscribers
  • Views 365 views
  • Users 0 members are here
Related

Cyclone II Max Clock Rate

bluesea
bluesea over 16 years ago

I am trying to get the most from my chip (EP2C20F484C7N). I have tried searching but everywhere seems to say different with no real reason to why that is the max rate.

In the datasheet from what I can see the max clock is 260Mhz.

However, I have found information to hint that it can go higher than this. For example, using both the rising and falling edge of the clock, PLL etc..

Can anyone share information on this?image

  • Sign in to reply
  • Cancel
  • edmund
    edmund over 16 years ago

    Hi,

     

    May I know which website did you come across that mention Cyclone II Max can support >260MHz. ? I am also curious on this too.

     

    Cheers

    Edmund

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago

    The max clking of an fpga is dependant on several things e.g. the fpga itself(including flipflop technology, routing...and other electrical level stuff that belongs to silicon people.) as well as the field engineers skill, design density speed density and the design itself(dedicated blocks usage and so on).
    It also may vary with different sections of same fpga.

    It is therefore hard for vendors to state exact figures but they only give an idea and in a comparative approach.

    The notion of using both edges is a trick to overcome clk speed limitation, usefull on board. You pass data at double clk speed onto two sets of registers but inside fpga ultimately a double clk is needed(clking one set of registers) to process data in their order.

    Your question on PLL: this is a different issue, you may generate fast clk but you need fpga to support that speed.

    • Cancel
    • Vote Up 0 Vote Down