Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum First 8-bit MCU with 128 KB Flash in a 28-pin Package
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 503 subscribers
  • Views 446 views
  • Users 0 members are here
  • 128k
  • 8-bit
  • microchip
  • 28-pin
  • flash
  • mcu
Related

First 8-bit MCU with 128 KB Flash in a 28-pin Package

GardenState
GardenState over 15 years ago

Many of today’s MCU applications require very low power consumption to extend battery life and reduce electricity demand. Microchip’s new PIC18F47J13PIC18F47J13 offers high memory density and low power in a small-footprint package to keep power budgets and BOM costs low.

The 8-bit MCU is said to be the industry’s first to feature 128 KB Flash program memory in a 28-pin package. Also available in a 44-pin package, the part uses Microship’s XLP (eXtreme Low Power) technology and incorporates mTouch capability for implementing capacitive touch sensing user interfaces and an on-chip 12-bit Analog-to-Digital Converter (ADC).

Pricing starts at $2.11 each, in 10,000-unit quantities.

  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    michaelkellett over 15 years ago

    It may be that in some cases the package is an advantage but I'm not sure that it is especially cheap - is it any cheaper than a STM32F100CB, ARM Cortex, 128k Flash, 48 pin with many nice peripherals on board including DAC, 12 bit ADC, CRC generator, DMA, etc etc.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 15 years ago

    It may be that in some cases the package is an advantage but I'm not sure that it is especially cheap - is it any cheaper than a STM32F100CB, ARM Cortex, 128k Flash, 48 pin with many nice peripherals on board including DAC, 12 bit ADC, CRC generator, DMA, etc etc.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • awneil
    awneil over 15 years ago in reply to michaelkellett
    If the application really requires 128K of flash, there's a fair chance that it isn't really suited to an 8-bit processor...