Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Circuit for controlling four piezoelectric sounders (without oscillator circuits) with one microcontroller pin
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 503 subscribers
  • Views 309 views
  • Users 0 members are here
Related

Circuit for controlling four piezoelectric sounders (without oscillator circuits) with one microcontroller pin

e14 Contributor
e14 Contributor over 14 years ago

Hi!

 

I am trying to control four piezoelectric sounders (without oscillator circuits) with one microcontroller pin (which can source about 20 mA of current).

 

The sounders are supposed to have a 12 V (peak-to-peak), so I tried a push pull configuration with transistors and an opamp. When I connected a piezoelectric sounder to the output of the push-pull circuit, it behaved like a short and fried the opamp.

Then I tried a normal opamp inverting amplifier. It seems to work for one or two, but I doubt it'll work for four.

 

The problem is that this has to be a low power (battery driven) solution, so an opamp that can be shut down (like the LT6000) is really important.

 

I don't have much space available on the PCB, so a compact solution is also important.

 

 

Does anyone know a good way to drive the piezoelectric elements?

  • Sign in to reply
  • Cancel

Top Replies

  • Leethal
    Leethal over 14 years ago +1
    Hi, I used the LM4860M/NOPB LM4860M/NOPB which is pretty much designed for that purpose.
Parents
  • Leethal
    Leethal over 14 years ago

    Hi,

     

    I used the LM4860M/NOPBLM4860M/NOPB which is pretty much designed for that purpose.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Leethal
    Leethal over 14 years ago

    Hi,

     

    I used the LM4860M/NOPBLM4860M/NOPB which is pretty much designed for that purpose.