Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum ARM + Video Streaming
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 503 subscribers
  • Views 1425 views
  • Users 0 members are here
Related

ARM + Video Streaming

e14 Contributor
e14 Contributor over 14 years ago

Hi guys,,, I'm new with embedded systems.. and I'd like to develop a video Streaming System with some ARM proccesor... the idea is using a webcam or some kind of camera to stream video over wifi .... any idea.. sugestion... I'm really new at this.... I have made some advaces with ffmpeg to coding the video... thanks

  • Sign in to reply
  • Cancel
Parents
  • robotonics
    robotonics over 14 years ago

    Hi

     

    I am just starting a new project...I am using a OV7670 Cmos camera module with the STM32F Discovery board , a 3.2 inch TFT touch screen,and a Wifi Bee.

     

    The OV7670 is a very good camera as it has a SCCB which is the same as I2C I am told, and will soon find out..In a week or so I will post results here...image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to robotonics

    I'm also working on this kind of project. So far I have an STM32F4Discovery board and an OV7670 camera

     

    https://lh3.googleusercontent.com/-8uC--zNxhNI/T46-3QdH04I/AAAAAAAAE-4/Ihs-Ck1NSpE/s400/IMG_20120418_031311.jpg

    I just finished making the camera work via DCMI, or at least I'm capturing frames but hard to tell without actually looking at a generated image. Do you guys have any idea how to view a bytestream of RGB565 data over serial port in a Windows PC? I can send the captured data to a serial port but I can't find a way to convert this data to a bitmap that can be displayed in the computer.

     

    Anyway, I'll be bookmarking this thread for any update.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to robotonics

    I'm also working on this kind of project. So far I have an STM32F4Discovery board and an OV7670 camera

     

    https://lh3.googleusercontent.com/-8uC--zNxhNI/T46-3QdH04I/AAAAAAAAE-4/Ihs-Ck1NSpE/s400/IMG_20120418_031311.jpg

    I just finished making the camera work via DCMI, or at least I'm capturing frames but hard to tell without actually looking at a generated image. Do you guys have any idea how to view a bytestream of RGB565 data over serial port in a Windows PC? I can send the captured data to a serial port but I can't find a way to convert this data to a bitmap that can be displayed in the computer.

     

    Anyway, I'll be bookmarking this thread for any update.