Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Which Microcontroller?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 504 subscribers
  • Views 819 views
  • Users 0 members are here
  • embedded
  • microcontroller
  • arm
  • pic
Related

Which Microcontroller?

rishi2628
rishi2628 over 11 years ago

I am a college student and I want to do a course on embedded system but i can't decide which microcontroller to choose. I already know AVR very well. Please help me decide out of PIC and ARM microcontroller. Which one is better and would help me boost my CV?

  • Sign in to reply
  • Cancel

Top Replies

  • johnbeetem
    johnbeetem over 11 years ago in reply to rishi2628 +2
    Rishi Sharma wrote: but sir this is arm microcontroller not arm processor. Should i still go with ARM? A microcontroller is a chip that includes a processor plus some combination of non-volatile…
  • clem57
    clem57 over 11 years ago +1
    I am taking a course on embedded microprocessors at Ux Austin on edx.org. Like @ John Beetem says, they are using a TI ARM processor. Check out the Wiki page to see what you think. Clem
  • clem57
    clem57 over 11 years ago in reply to rishi2628 +1
    To clarify a bit, The ARM instructions can be used with Axx microprocessors and with Mx microcontrollers. The TI version is a microcontroller(M3) with 43 pins supporting digital, analog, uart(serial),…
Parents
  • johnbeetem
    johnbeetem over 11 years ago

    I'd go with ARM.  There are dozens of semiconductor vendors selling ARM processors of various sizes and prices and power consumption, so you have lots of flexibility.  There are also lots of cheap ARM development boards.  With PIC you have a single vendor.

     

    ARM is a fun architecture.  There are many variants so you get to learn all sorts of fun things like Thumb and Thumb-2, not to mention the 64-bit ARMv8.  ARM is a whole computer architecture course all in one family image

     

    JMO/YMMV

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rishi2628
    rishi2628 over 11 years ago in reply to johnbeetem

    but sir this is arm microcontroller not arm processor. Should i still go with ARM?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 11 years ago in reply to rishi2628

    To clarify a bit, The ARM instructions can be used with Axx microprocessors and with Mx microcontrollers. The TI version is a microcontroller(M3) with 43 pins supporting digital, analog, uart(serial), I2C, SPI , and PWM interfaces. They even support ADC as well as DAC interfaces. The other choice is ATMEL like Arduino flavors. These are mostly hobbyists. Pic is another set from MicroChips.

     

    Hope this helps,

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • clem57
    clem57 over 11 years ago in reply to rishi2628

    To clarify a bit, The ARM instructions can be used with Axx microprocessors and with Mx microcontrollers. The TI version is a microcontroller(M3) with 43 pins supporting digital, analog, uart(serial), I2C, SPI , and PWM interfaces. They even support ADC as well as DAC interfaces. The other choice is ATMEL like Arduino flavors. These are mostly hobbyists. Pic is another set from MicroChips.

     

    Hope this helps,

    Clem