Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum ARM Programming
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 4 answers
  • Subscribers 505 subscribers
  • Views 987 views
  • Users 0 members are here
  • arm
Related

ARM Programming

rishi2628
rishi2628 over 10 years ago

I am a high school student, who is experienced in Arduino and AVR Programming. Now I want to extend my abilities and go for ARM. Could anyone please suggest me a website or from where I can learn ARM Programming on my own. I don't care about the company of the ARM Processor. I just want to learn the programming, whether it is STM , Nuvaton, etc,etc. Please suggest something. It means a lot to me. Thank you. image

  • Sign in to reply
  • Cancel

Top Replies

  • mconners
    mconners over 10 years ago +5 suggested
    You may want to check this course out edX Embedded Systems Course It's a good class, there are probably archived versions of an earlier class. Also, this book, http://www.cs.indiana.edu/~geobrown/book…
  • clem57
    clem57 over 10 years ago +3 suggested
    I would start at a hardware level like ARM Assembly Language Programming . This should be followed with an IDE like Energia since it is very like Arduino except geared for ARM. Hope this helps. Of course…
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to clem57 +3 suggested
    Clem, I agree with your syarting point. As you mention energia I think you are suggesting the msp boards and the entire TI echosystem. That is great for arm and also for the wide range of available boards…
Parents
  • johnbeetem
    0 johnbeetem over 10 years ago

    Most ARM programmers program in C.  The ARM machine language is designed to be compiled from C, and there's rarely a need to program in ASM since you can get at almost all machine features using C.

     

    However, if you're interested in broadening your programming knowledge, ASM can be exhilarating since you are programming at the bare metal and telling the CPU exactly what to do.  It's like reading a foreign language work in its original form instead of someone else's translation.

     

    ASM can also be very frustrating, especially for a beginning.  As I wrote in another thread:

    People sometimes refer to C as "programming without seatbelts".  Well, ASM is "programming without seats, lights, brakes, tires, or a even a body".

    ARM ASM is not a simple assembly language.  At one time ARM stood for Acorn RISC Machine, and later Advanced RISC Machine.  Now ARM doesn't stand for anything.  Each new architecture version added new instructions into the holes in the previous architectures, ending up with a "dog's breakfast" of an instruction set.  One of the requirements of a RISC architecture is a few simple instruction formats.  Well, the last ARM ARM (ARM Architecture Reference Manual) that had a table of instruction formats was ARMv5.  ARMv7 has so many instruction formats (especially by adding Thumb2) that they've given up on having a consolidated instruction format table.

     

    So if you haven't programmed ASM before, I wouldn't recommend ARM as a starting point.  FWIW, my favorites are PDP-11, 68000/Coldfire, and PowerPC.  I haven't done any actual MSP430 programming, but the instruction set looks a lot like my beloved PDP-11.

     

    Here are a couple of discussions you might find interesting.  This one at raspberrypi.org includes links to the ARM corporation site where you can download ARM ARMs.  This one at element14 is an entertaining free-wheeling discussion of what's the best first programming language and includes some interesting discussion of ASM in general and includes my quote from above.

     

    Hope this helps!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • johnbeetem
    0 johnbeetem over 10 years ago

    Most ARM programmers program in C.  The ARM machine language is designed to be compiled from C, and there's rarely a need to program in ASM since you can get at almost all machine features using C.

     

    However, if you're interested in broadening your programming knowledge, ASM can be exhilarating since you are programming at the bare metal and telling the CPU exactly what to do.  It's like reading a foreign language work in its original form instead of someone else's translation.

     

    ASM can also be very frustrating, especially for a beginning.  As I wrote in another thread:

    People sometimes refer to C as "programming without seatbelts".  Well, ASM is "programming without seats, lights, brakes, tires, or a even a body".

    ARM ASM is not a simple assembly language.  At one time ARM stood for Acorn RISC Machine, and later Advanced RISC Machine.  Now ARM doesn't stand for anything.  Each new architecture version added new instructions into the holes in the previous architectures, ending up with a "dog's breakfast" of an instruction set.  One of the requirements of a RISC architecture is a few simple instruction formats.  Well, the last ARM ARM (ARM Architecture Reference Manual) that had a table of instruction formats was ARMv5.  ARMv7 has so many instruction formats (especially by adding Thumb2) that they've given up on having a consolidated instruction format table.

     

    So if you haven't programmed ASM before, I wouldn't recommend ARM as a starting point.  FWIW, my favorites are PDP-11, 68000/Coldfire, and PowerPC.  I haven't done any actual MSP430 programming, but the instruction set looks a lot like my beloved PDP-11.

     

    Here are a couple of discussions you might find interesting.  This one at raspberrypi.org includes links to the ARM corporation site where you can download ARM ARMs.  This one at element14 is an entertaining free-wheeling discussion of what's the best first programming language and includes some interesting discussion of ASM in general and includes my quote from above.

     

    Hope this helps!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer