Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Prevent backfeeding from arduino 5V pin
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Answers 3 answers
  • Subscribers 505 subscribers
  • Views 1622 views
  • Users 0 members are here
Related

Prevent backfeeding from arduino 5V pin

steve25
steve25 over 9 years ago

Hi all,

 

I have a problem with my arduino nano board. The 5V pin is backfeeding into my circuit when i plugin my USB cable. My circuit draws way to much current than my USB can supply. So the question is: Is there a way to prevent the backfeeding into my circuit? I already considered using diodes but that would create a voltage drop of 0,7V which is a bit much.

 

Hope i'l get a response soon!

 

Steve

  • Sign in to reply
  • Cancel

Top Replies

  • D_Hersey
    D_Hersey over 9 years ago +1 suggested
    Shottky or Ge?
Parents
  • D_Hersey
    0 D_Hersey over 9 years ago

    Shottky or Ge?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • steve25
    0 steve25 over 9 years ago in reply to D_Hersey

    Thanks for the reply. A Schottky is a good solution because of the low forward voltage. But I think i'l use a transistor. I connect the base to an external power source line. So if the external power source isn't on the transistor is turned off. The 5v pin can't backfeed in this case!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • steve25
    0 steve25 over 9 years ago in reply to D_Hersey

    Thanks for the reply. A Schottky is a good solution because of the low forward voltage. But I think i'l use a transistor. I connect the base to an external power source line. So if the external power source isn't on the transistor is turned off. The 5v pin can't backfeed in this case!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer