Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Can anyone here give me an idea about a closed loop small arduino project?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 5 answers
  • Subscribers 504 subscribers
  • Views 1159 views
  • Users 0 members are here
  • control systems
  • wireless controller
Related

Can anyone here give me an idea about a closed loop small arduino project?

mhanzala507
mhanzala507 over 8 years ago

My professor assigned me a project which i have to choose on my on. I t should be a closed loop circuit, means input is applied and a sensor checks the output and if there is any deficiency it increase or decrease the input.

I had an idea of controlling an actual ceiling fan. It should be temperature controlled and must e automatic. when a person enters the room the light as well as fan must starts automatically and when person leaves the room it must turn off automatically.

I don't have any idea how to do this all stuff.

Suggest me another good project or help me out with this project. 

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 8 years ago +3 suggested
    I’ve written a blog post here on e14 about porting an Arduino PID library to another platform. The blog contains a link to that very good library. MSP432 and TI-RTOS: PID Library Part 1 - Intro
  • jw0752
    jw0752 over 8 years ago +2 suggested
    Hi Muhammad, I'm not sure your proposed project is closed loop. Isn't that more like having a container of water with a leak. When the water gets below a certain level a sensor is triggered and it starts…
  • dougw
    dougw over 8 years ago +2 suggested
    A closed loop refers to a control system where the output is adjusted to achieve a target condition based on feedback from a sensor. If the sensor indicates the condition is below target the output gets…
Parents
  • dougw
    0 dougw over 8 years ago

    A closed loop refers to a control system where the output is adjusted to achieve a target condition based on feedback from a sensor. If the sensor indicates the condition is below target the output gets increased and vice versa.

    Temperature control is a great example where a temperature sensor is used to determine if the temperature needs to go up or down to reach a desired temperature.

    However a fan is not very good at changing the temperature - it moves air but does not change the temperature of the air. If the air supply is hotter or cooler than ambient, a fan can be used to change ambient temperature to be closer to the air supply temperature. But it needs a heater or an air conditioner to control temperature.

    A simpler project might be to control the temperature of water in a bucket, using a heater and a temperature sensor.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • dougw
    0 dougw over 8 years ago

    A closed loop refers to a control system where the output is adjusted to achieve a target condition based on feedback from a sensor. If the sensor indicates the condition is below target the output gets increased and vice versa.

    Temperature control is a great example where a temperature sensor is used to determine if the temperature needs to go up or down to reach a desired temperature.

    However a fan is not very good at changing the temperature - it moves air but does not change the temperature of the air. If the air supply is hotter or cooler than ambient, a fan can be used to change ambient temperature to be closer to the air supply temperature. But it needs a heater or an air conditioner to control temperature.

    A simpler project might be to control the temperature of water in a bucket, using a heater and a temperature sensor.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer