Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Maximize the Sound from a Buzzer
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 14 replies
  • Answers 7 answers
  • Subscribers 505 subscribers
  • Views 9400 views
  • Users 0 members are here
  • buzzer
  • alarm
Related

Maximize the Sound from a Buzzer

fmilburn
fmilburn over 8 years ago

I am working on a gizmo that will alert the user to an event using sound and light.  It will be in a small enclosure.  My objective is to make the buzzer as loud and annoying as possible, with an option to soften it. This is what I have to work with power wise:

 

  • 5V from USB
  • 3V logic from microcontroller
  • gizmo will include a radio so want to avoid a switching boost converter

 

I put together the following circuit on a breadboard which works more or less as expected:

 

image

I don't need to vary pitch and the buzzer I just happened to have on hand is an active buzzer (that is to say it will buzz with only DC) which frees up a timer on the microcontroller.  I have looked through the E14 offerings and 85 dB seems to be about the best I can expect at 5V.  Before I blindly pick one and move on here are my observations and questions:

 

1) There is a sharp transition between loud and soft.  It seems subjectively like it goes from a soft buzz to full throttle with a small change in R5 on the schematic.

2) Are there high efficiency buzzers I am missing or is the only way to get higher volume with higher power and thus, higher voltage.

3) I might consider an amplifier with speaker but it would have to be simple, sturdy, and compact.

 

Thoughts and ideas are greatly appreciated!

 

Frank

Attachments:
image
  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 8 years ago +5 suggested
    Piezo buzzers will provide higher sound pressure level with lower input power than magnetic buzzers. The input power is minimized and the output sound pressure level is maximized when the buzzer is operating…
  • dr-jhc
    dr-jhc over 8 years ago +5 suggested
    Another option could be to do something mechanical to provide better impedance-matching of the buzzer to the air: essentially some way to make the buzzer move air more efficiently. Some kind of waveguide…
  • shabaz
    shabaz over 8 years ago +5 suggested
    Hi Frank, Interesting topic I've looked in the past for good buzzer circuits too, and it seems quite hard to find an off-the-shelf single chip to do this these days. One trick I recall was to use a schmitt…
Parents
  • fmilburn
    0 fmilburn over 8 years ago

    Thanks again for the great response to my question and the help provided.  There is a preliminary schematic posted here that shows the current state of the circuit I am building:  AIS Alarm - Schematic

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • fmilburn
    0 fmilburn over 8 years ago

    Thanks again for the great response to my question and the help provided.  There is a preliminary schematic posted here that shows the current state of the circuit I am building:  AIS Alarm - Schematic