Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Very new design person here needing some input
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Answers 3 answers
  • Subscribers 505 subscribers
  • Views 946 views
  • Users 0 members are here
  • pcb board
  • custom pcb
Related

Very new design person here needing some input

katghoti
katghoti over 8 years ago

I am creating a project that uses a Raspberry Pi Zero W and an ultrasonic distance measuring device (HC-SR04).  I have the code done, but now I want to move from the motherboard to a small PCB that will let me hook up the tester quickly.

 

Here is a layout I pulled from the web that shows the need to split the signal back to ground to 3.3 volts do it doesn't fry the Pi.

 

image

 

So I took a stab a designing my first PCB using Autodesk eagle.  It was a struggle, but I think I got it done.  Here is a screenshot of the finished board

 

image

 

 

 

On one side I have the pins to match the Ultrasonic-module (IN) and one set of pins to go to the PI (OUT).  I am using a 1K AND 2K resistor on the advice of another post to split the signal back.  Before I send this out to get a PCP bid, can someone with vastly more knowledge than I look it over quickly and make sure this is correct according to the layout above.  I am working on a silkscreen layer for the pins on both sides to help with hookup, but right now I just need to know if I am on the right track.

 

Thanks.

 

John

  • Sign in to reply
  • Cancel

Top Replies

  • genebren
    genebren over 8 years ago +3 verified
    John, Your PCB looks OK. I say this not completely understanding which pins on your 'IN' and 'OUT' are assigned to. Just guessing at this point but the 'OUT' side looks like Ground, Echo, +5v or Trigger…
  • katghoti
    katghoti over 8 years ago in reply to thehwcave +3
    I had not considered this path. Although it was fun creating the PCB, I think I will take a look a this route. It looks less expensive and should do what I need. Thank you very much!. John
  • katghoti
    katghoti over 8 years ago in reply to genebren +2
    Yes the in side will match up (from the bottom up) +5V, Trigger, Echo, Ground coming from the ultrasonic tester. The out side will be 5V from the pi, GPIO PIN, GPIO PIN, Ground. The GPIO pins will vary…
Parents
  • thehwcave
    0 thehwcave over 8 years ago

    Hi John,

    just wondering, making a PCB for such a small circuit seems to be a lot of work. I would just use piece of Veroboard (aka stripboard) ...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • katghoti
    0 katghoti over 8 years ago in reply to thehwcave

    I had not considered this path.  Although it was fun creating the PCB, I think I will take a look a this route.  It looks less expensive and should do what I need.

     

    Thank you very much!.

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • katghoti
    0 katghoti over 8 years ago in reply to thehwcave

    I had not considered this path.  Although it was fun creating the PCB, I think I will take a look a this route.  It looks less expensive and should do what I need.

     

    Thank you very much!.

     

    John

    • Cancel
    • Vote Up +3 Vote Down