Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum What is Arduino?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 498 subscribers
  • Views 645 views
  • Users 0 members are here
  • 8_bit
  • avr
  • ide
  • microprocessors
  • atmega
  • 32_bit
  • hardware
  • 16_bit
  • microcontrollers
  • embedded
  • Design
  • mcu
  • mpu
  • arduino
  • atmel
  • software
Related

What is Arduino?

e14 Contributor
e14 Contributor over 16 years ago

There appears to be a lot of interest and groups actively working with Arduino at individual level and within education segment.

Strangely though, why is it so few within major semiconductor brands know anything about this?

Any experience, expertise, knowledge out there would be welcome, especially if there is some easy material to work with.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 16 years ago

    Arduino is a simple hardware and software system based on Atmel AVR microcontrollers with a bootloader and the simple Wiring programming language and Processing IDE.  The device can be programmed without the need for a seperate programmer.

    It's intended to make the implementation of electronics easier for those not familiar with electronics, such as artists, but has been widely adopted within the hobbyist community.  Many different 'shields' are available to add additional features to the basic development boards, such as ethernet or motor control.

    There are also many different Arduino clone boards available, with differnet board layouts, features or microcontrollers, which are compatible with all shields as well as the bootloader.

    http://www.arduino.cc has tons more information.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 16 years ago

    Arduino is a simple hardware and software system based on Atmel AVR microcontrollers with a bootloader and the simple Wiring programming language and Processing IDE.  The device can be programmed without the need for a seperate programmer.

    It's intended to make the implementation of electronics easier for those not familiar with electronics, such as artists, but has been widely adopted within the hobbyist community.  Many different 'shields' are available to add additional features to the basic development boards, such as ethernet or motor control.

    There are also many different Arduino clone boards available, with differnet board layouts, features or microcontrollers, which are compatible with all shields as well as the bootloader.

    http://www.arduino.cc has tons more information.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data