Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Thought Experiment; Detecting Distance
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 37 replies
  • Answers 5 answers
  • Subscribers 506 subscribers
  • Views 3644 views
  • Users 0 members are here
  • embedded
  • development
  • mcu
  • puzzle
Related

Thought Experiment; Detecting Distance

Catwell
Catwell over 16 years ago
We have two blocks, A & B shown below, moving away from each other. How can one detect that the separation has reached a certain point, distance X in this case?
 
The most obvious solution is two rods, one on each block, that make contact when the distance is X. But this is a crude and cumbersome option. It's 2010, how about a high tech solution?

image

 
 
There is no right or wrong, just an excellent chance to work out the prefrontal cortex and showing off some creativity.
  • Sign in to reply
  • Cancel

Top Replies

  • DAB
    DAB over 14 years ago +1
    Hi Cabe, A very simple approach is to set up two laser pointers set up to hit the same spot at only the correct distance. As you move one box towards the other, the two laser spots will converge. If you…
Parents
  • albertosombri
    0 albertosombri over 16 years ago

    Hi Cabe,

    yes I have experience in developing US system.

    some years ago I developed an Electronic Parking System, it works just like a bat sense.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Catwell
    0 Catwell over 16 years ago in reply to albertosombri

    In an ideal situation Ultrasonic might be perfect. However, what if it is in a noisy industrial environment? Is there a way to isolate the signal?

     

    Also, please post some links to the Ultrasonic emitter/detectors you've used.

     

    Thanks.

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Catwell
    0 Catwell over 16 years ago in reply to albertosombri

    In an ideal situation Ultrasonic might be perfect. However, what if it is in a noisy industrial environment? Is there a way to isolate the signal?

     

    Also, please post some links to the Ultrasonic emitter/detectors you've used.

     

    Thanks.

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • albertosombri
    0 albertosombri over 16 years ago in reply to Catwell

    Something about US system.

     

    In the 1994 we developed a US system for FIAT car alarm system, the goal was to detect any movments inside the car, when the car was parked.

    So we built up a small 44KHz transmitter, using analog components, and also an analog receiver able to detect signal phase variations.

     

    In the 2004 I worked in another company and we developed an electronic parking system with US technology. We always used discrete devices for TX and Rx, then a uP able to measure the delay between the transmitted signal and the received signal.

     

    Alberto.