Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Thought Experiment; Detecting Distance
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 37 replies
  • Answers 5 answers
  • Subscribers 506 subscribers
  • Views 3675 views
  • Users 0 members are here
  • embedded
  • development
  • mcu
  • puzzle
Related

Thought Experiment; Detecting Distance

Catwell
Catwell over 16 years ago
We have two blocks, A & B shown below, moving away from each other. How can one detect that the separation has reached a certain point, distance X in this case?
 
The most obvious solution is two rods, one on each block, that make contact when the distance is X. But this is a crude and cumbersome option. It's 2010, how about a high tech solution?

image

 
 
There is no right or wrong, just an excellent chance to work out the prefrontal cortex and showing off some creativity.
  • Sign in to reply
  • Cancel

Top Replies

  • DAB
    DAB over 15 years ago +1
    Hi Cabe, A very simple approach is to set up two laser pointers set up to hit the same spot at only the correct distance. As you move one box towards the other, the two laser spots will converge. If you…
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Late joiner!

     

    I would recommend capacitance, assuming (1) there is an opportunity to calibrate and (2) the environment is fairly free of non-repeatable (i.e., cannot be captured during calibration) outside influences. Block A has active electronics on it. Block B has a metal (foil works) plate on the side facing Block A. Block A includes one plate of a capacitor, a driven shield for that plate, and a ground "plate" (consisting of a ring of foil around the perimeter of the side facing Block B).

     

    The field from the driven center plate to the grounded perimeter is forced to extend fairly far out into space. The disturbance by the foil on Block B alters the capacitance between the center plate and ground. Measure the capacitance (there are various ways) vs. distance to establish a calibration curve and you are done. This is fairly immune to temperature, very susceptible to dielectric constant change of the intervening material, and very cheap to build (under $30 in electronics - voice of experience!). One part in 400 is not too difficult to do with a 2nd order curve fit (8-bit microcontroller is sufficient, but a math library helps!), but accuracy also depends on movement being restricted to X direction.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Late joiner!

     

    I would recommend capacitance, assuming (1) there is an opportunity to calibrate and (2) the environment is fairly free of non-repeatable (i.e., cannot be captured during calibration) outside influences. Block A has active electronics on it. Block B has a metal (foil works) plate on the side facing Block A. Block A includes one plate of a capacitor, a driven shield for that plate, and a ground "plate" (consisting of a ring of foil around the perimeter of the side facing Block B).

     

    The field from the driven center plate to the grounded perimeter is forced to extend fairly far out into space. The disturbance by the foil on Block B alters the capacitance between the center plate and ground. Measure the capacitance (there are various ways) vs. distance to establish a calibration curve and you are done. This is fairly immune to temperature, very susceptible to dielectric constant change of the intervening material, and very cheap to build (under $30 in electronics - voice of experience!). One part in 400 is not too difficult to do with a 2nd order curve fit (8-bit microcontroller is sufficient, but a math library helps!), but accuracy also depends on movement being restricted to X direction.