Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Thought Experiment; Detecting Distance
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 37 replies
  • Answers 5 answers
  • Subscribers 506 subscribers
  • Views 3668 views
  • Users 0 members are here
  • embedded
  • development
  • mcu
  • puzzle
Related

Thought Experiment; Detecting Distance

Catwell
Catwell over 16 years ago
We have two blocks, A & B shown below, moving away from each other. How can one detect that the separation has reached a certain point, distance X in this case?
 
The most obvious solution is two rods, one on each block, that make contact when the distance is X. But this is a crude and cumbersome option. It's 2010, how about a high tech solution?

image

 
 
There is no right or wrong, just an excellent chance to work out the prefrontal cortex and showing off some creativity.
  • Sign in to reply
  • Cancel

Top Replies

  • DAB
    DAB over 15 years ago +1
    Hi Cabe, A very simple approach is to set up two laser pointers set up to hit the same spot at only the correct distance. As you move one box towards the other, the two laser spots will converge. If you…
Parents
  • billpenner
    0 billpenner over 15 years ago

    By mounting a laser on the far edge of block  A, a reflecter on block B and a detecter on the near side of block A. Assuming stability of the blocks, the distance between the laser and the detector sets  the stop point. (distance between blocks)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to billpenner

    Another method that could be used in conjunction with billpenner's reflection / triangulation method is laser pulse generation. A rapid pulse is needed, and if you measure the rise time on the pulse, and the rise time on the reflected / detected pulse, you can calculate distance through phase difference.

     

    Quick calculations / thoughts

    Speed of light in a vacuum: 299798458 metres per second (c - 90 for light speed through air)

    So, 1 / (299798458 - 90) = 3.335575196 nS per metre.

    Therefore, if you want to measure with metre accuracy, you'd have to have pulse detection down to 3.3nS. 10cm? 330pS. Hmm... What you might be able to do is generate a longer pulse, but proportional to the received pulse difference duration. This scaling might also allow for tuning. 1GHz / 1nS isn't so difficult to build for, maybe 2, so this approach might be doable.

     

    It would also translate well to longer distances, where trigonometric methods would have to measure increasingly shallow angles - on the contrary here, the pulse delay is longer, and therefore easier to detect.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    Of course, if you're doing this with a reflector, 3.33nS would give you 50CM resolution, as the light will travel there then back - an increase of 1M distance then means 2M extra round trip. Again, doubling the time makes it a bit easier to detect perhaps.

     

    My apologies - I came straight to the 2nd page! Laser interferometry too expensive then... Ok, well using a laser pointer as a previous poster suggested, with a reflector, might be the way forward. As the blocks are also fairly close, an old barcode scanner might be an ideal source of parts; The internals often use a sensor that's effectively a single line cmos / ccd camera. This could be used to determine the angle of reflection quite easily, and also be an easily adjustable / configurable solution.

     

    Ultrasonics might be a good way forward too, but you could also use an LED driven by a tone generator - a phototransistor might then be used to determine distance based on either amplitude of the reflected signal, or angle, dependent on placement / focus / surface reflectivity.

     

    Hope that helps some more! image

     

    Further to the above, the PIC24F64GB004 (and others) have a CTMU peripheral. This is capable of 1nS resolution & generating pulses asyncronously w.r.t. the internal clock. So, laser ranging may still be possible on a budget! (1M = 2M round trip of 6.6nS, therefore 1 / 6.6 = 15.15CM resolution @ 1nS) Perhaps not for the 250 microns you'd ideally like for your setup though. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Catwell
    0 Catwell over 15 years ago in reply to e14 Contributor

    Billpenner & Frost,

     

    I like the lasr range finder option most. Although I was looking for a simpler answer, I think this may work out well.

    Some thoughts on how to actually build such a device? If it isn't too expensive, I will attempt to build it.

     

    The theory:

    image

    Distance = h / tan(theta)

     

    This is what you are proposing?

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to Catwell

    Your picture is pretty much what I thought, except the laser would need to be set at angle theta, on the "source" block. Movments on the target block away / towards source would then change where the reflected laser point hit the target.

     

    Either way, you've got a mirror / reflector / angle problem to solve. Setting theta for the laser shouldn't be too hard - simply accurately measure a right angled triangle inside a large room, the triangle is of known proportions, bingo, you've got a known theta.

     

    The other way is to get a reflector set at angle theta on the target block. A little bit harder, and if it's moving, it may change the angle and destroy accuracy. If you use a flat mirror on the target, it's probably simpler all round.

     

    Anyway, it looks like the final calc is going to be distance = (h/2) / tan(theta) as your diagram would appear to show the beam reflecting off a surface with a mirror set at theta degrees.

     

    So, detecting where the laser pointer hits is the last problem to solve. Preferably, I suppose you'd use as few optical components as possible as that way is going to be expensive, due to accuracy depending on quality and ability to set correctly. Simplest option I can think of is to print off a scale on a laser printer / A4 paper, and use this for the beam to hit and for a camera to see. Software can then determine where the beam is hitting, maybe even without a printed scale, and convert to distance.

     

    In my opinion, using software to do the bulk of the work is going to be the best / cheapest way in terms of physical cost, apart from perhaps time. All you'd need to do though is detect at what point the colour thresholds exceed a certain value, in the X and Y planes. A camera looking at the back of the sheet of paper should do this ok. Classes are available in both .NET and Java to do this, depending on your preference.

     

    For more accuracy this way, the simplest method is to make angle theta more obtuse, therefore affecting h more over a given distance. To calibrate such a device, measure distance D at two points with calipers, and then mark the spot positions (in software / on paper / however) as required. Determining distance between these two points should be a simple matter of interpolation.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • billpenner
    0 billpenner over 14 years ago in reply to Catwell

    I know this is old but just ran across some Light to frequency converters. With a resolution of 16 bits and a wide range of sensitivities, Looks as if this might be the low cost answer. Please check taosinc.com for more info.The available devices include both analog and digital.Some with programmable gain. for a wide range of light sensitivity. Couple this with a reflectivity of block A or source on block A with sensor on block B, the range can can be varied. Also using an adjustable light source, the distance can be varied over a wide range. The cost of the sensors are only a couple bucks. I am going to build a motion sensor using one of the analog as well as one of the digital sensors. I have a need to measure the absolute speed of motion of an object independent of direction. Sorry for the long response time.

    Bill

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • billpenner
    0 billpenner over 14 years ago in reply to Catwell

    I know this is old but just ran across some Light to frequency converters. With a resolution of 16 bits and a wide range of sensitivities, Looks as if this might be the low cost answer. Please check taosinc.com for more info.The available devices include both analog and digital.Some with programmable gain. for a wide range of light sensitivity. Couple this with a reflectivity of block A or source on block A with sensor on block B, the range can can be varied. Also using an adjustable light source, the distance can be varied over a wide range. The cost of the sensors are only a couple bucks. I am going to build a motion sensor using one of the analog as well as one of the digital sensors. I have a need to measure the absolute speed of motion of an object independent of direction. Sorry for the long response time.

    Bill

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Catwell
    0 Catwell over 14 years ago in reply to billpenner

    Brilliant ideas. All worth trying.

     

    Timatthelab, would block B's foil still be affected to a detectable margin at far distances. Say, at 20cm?

     

    Saturation, I can not wait to try the light range finder option.

     

    Billpenner, I am going to look into your option.

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to Catwell

    The range for capacitance measurements depends primarily on the geometry, of which the distance is a big part. I have found that the usable range is about 1 to 3 times the diameter of the electrode "plate" used. In this case, one plate is the center sensor, while the other is the ground ring, complicated by the "reflection" off of the Block B target. With sufficient width of the ground ring, one could expect decent results to about 2 to 3 times the sensor diameter. If you get much farther than that, the amount of gain required is so great that the noise become problematic (although you can recover from it to a point if you can average over a long enough time).

     

    Also, note that Block B does not necessarily need a foil, if it's dielectric constant is sufficiently high. E.g., the raw material used in soylent green is full of water, so you can use this technique as a decent "person detector".