Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Thought Experiment; Detecting Distance
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 37 replies
  • Answers 5 answers
  • Subscribers 506 subscribers
  • Views 3650 views
  • Users 0 members are here
  • embedded
  • development
  • mcu
  • puzzle
Related

Thought Experiment; Detecting Distance

Catwell
Catwell over 16 years ago
We have two blocks, A & B shown below, moving away from each other. How can one detect that the separation has reached a certain point, distance X in this case?
 
The most obvious solution is two rods, one on each block, that make contact when the distance is X. But this is a crude and cumbersome option. It's 2010, how about a high tech solution?

image

 
 
There is no right or wrong, just an excellent chance to work out the prefrontal cortex and showing off some creativity.
  • Sign in to reply
  • Cancel

Top Replies

  • DAB
    DAB over 14 years ago +1
    Hi Cabe, A very simple approach is to set up two laser pointers set up to hit the same spot at only the correct distance. As you move one box towards the other, the two laser spots will converge. If you…
Parents
  • e14 Contributor
    0 e14 Contributor over 16 years ago

    It would take some doing to get .25% accuracy with ultrasound.  You have to fight 3 different problems:

    1. Speed of sound changes with temperature (very roughly .1% every degree F), you could correct for that with a temperature sensor, so it's not too bad.

    2. Speed of sound changes with humidity (bone dry to saturated might be about .5% difference (again very roughly) in a warm environment, again, humidity sensor could take care of that.

    3. Speed of sound changes with gas composition, measuring that would be tricky, but it's not a huge factor, but can be noticable.

     

    Also note if your environment is windy you'll have to go with two transducers instead of reflections to correct for it.

     

    Ultrasound is great for getting a good idea of distance, but getting serious accuracy out of it takes some work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 16 years ago

    It would take some doing to get .25% accuracy with ultrasound.  You have to fight 3 different problems:

    1. Speed of sound changes with temperature (very roughly .1% every degree F), you could correct for that with a temperature sensor, so it's not too bad.

    2. Speed of sound changes with humidity (bone dry to saturated might be about .5% difference (again very roughly) in a warm environment, again, humidity sensor could take care of that.

    3. Speed of sound changes with gas composition, measuring that would be tricky, but it's not a huge factor, but can be noticable.

     

    Also note if your environment is windy you'll have to go with two transducers instead of reflections to correct for it.

     

    Ultrasound is great for getting a good idea of distance, but getting serious accuracy out of it takes some work.