Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Thought Experiment; Detecting Distance
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 37 replies
  • Answers 5 answers
  • Subscribers 506 subscribers
  • Views 3640 views
  • Users 0 members are here
  • embedded
  • development
  • mcu
  • puzzle
Related

Thought Experiment; Detecting Distance

Catwell
Catwell over 16 years ago
We have two blocks, A & B shown below, moving away from each other. How can one detect that the separation has reached a certain point, distance X in this case?
 
The most obvious solution is two rods, one on each block, that make contact when the distance is X. But this is a crude and cumbersome option. It's 2010, how about a high tech solution?

image

 
 
There is no right or wrong, just an excellent chance to work out the prefrontal cortex and showing off some creativity.
  • Sign in to reply
  • Cancel

Top Replies

  • DAB
    DAB over 14 years ago +1
    Hi Cabe, A very simple approach is to set up two laser pointers set up to hit the same spot at only the correct distance. As you move one box towards the other, the two laser spots will converge. If you…
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    What about String-pots?

    http://www.unimeasure.com/

     

    With a little bit of calibration/interpolation, you can probably achieve the accuracy you're after

     

    Or LVDTs?

    http://www.lvdt.co.uk/pdf/AML-E.pdf

     

    Or finally magnetic encoders;

    http://www.renishaw.com/en/magnetic-linear-encoders-and-magnetic-ring-encoders--9802

     

    Any of those are simpler/easier to implement that optical or US solutions, and should give you the kind of accuracy you're after.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    String pots aren't a bad idea, except when you have to worry about humidity changes and string stretch.  Good for being able to replace them though, and wouldn't be too hard to implement a centering capability with end cap limit switches.  The LVDT's are quite a bit more accurate, IMHO, used them for flight control position sensing on Helicopters.  Currently work with encoders and wheels that measure speed/distance for conveyor belts.  They work well if you can find the right combination to get the 7.5 degree measurements to equal a specific linear measurement. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Regular calibration (yearly) should take care of any stretch in the steel wire used for the pots strings.. not sure how humidity would affect that. (temperature is likely to much bigger effect).

     

    As for the encoders, take a look at the link.. I meant linear magnetic encoders, they use magnetic strips with alternating poles with a moving reader head. the accuracy can be down to a micron if required, 20microns is quite common (0.02mm). Bit more difficult to use but worth it if accuracy and reliability is what you need

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Regular calibration (yearly) should take care of any stretch in the steel wire used for the pots strings.. not sure how humidity would affect that. (temperature is likely to much bigger effect).

     

    As for the encoders, take a look at the link.. I meant linear magnetic encoders, they use magnetic strips with alternating poles with a moving reader head. the accuracy can be down to a micron if required, 20microns is quite common (0.02mm). Bit more difficult to use but worth it if accuracy and reliability is what you need