Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum 3A+ 3Phase Motor Controller
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 3 answers
  • Subscribers 503 subscribers
  • Views 943 views
  • Users 0 members are here
  • 32bit
  • 8_bit
  • 32_bit
  • 16_bit
  • 3-phase
Related

3A+ 3Phase Motor Controller

Catwell
Catwell over 16 years ago

IC based brushless 3-phase motor controllers are on the rise, though I am not sure what is available past remote control airplane drive circuitry.

 

I want an IC that has the commutation functions built in, H-bridge built it, and anything above that would be welcomed icing on the cake.

 

One requirement, I need 3A+ on each phase.

 

What is available these days?

 

Cabe

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 16 years ago

    If you can afford the board space and want 5-10A, the Maxon DEC 50/5 OEM module is one option for sensored motors. Though not an IC, it is an integrated module that is relatively compact.

     

    http://www.maxonmotorusa.com/media_releases_10439.html

     

    It has some very nice features, runs up to 50V, and requires almost no external components.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Catwell
    0 Catwell over 16 years ago in reply to e14 Contributor

    Shane,

     

    The board looks good too. I like the options it has. However, space is very limited for the project.

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Catwell
    0 Catwell over 16 years ago in reply to e14 Contributor

    Shane,

     

    The board looks good too. I like the options it has. However, space is very limited for the project.

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to Catwell

    Here is another very interesting new integrated 3-phase motor driver chip:

     

    http://focus.ti.com/lit/ds/symlink/drv8332.pdf