Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Design Challenge : accurately measure several liquids in a container
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 502 subscribers
  • Views 858 views
  • Users 0 members are here
  • design_challenge
  • desgin
  • microcontrollers
  • microcontroller
  • programmable_logic
  • software
Related

Design Challenge : accurately measure several liquids in a container

Catwell
Catwell over 15 years ago
It has been a while since my last Design Challenge to the community, but it's time to get back into the groove and working the prefrontal cortex. Innovation is spurred through creative thinking, so give it a shot even if you don't reply.
 
Similar to one I proposed in the past, Measuring liquid inside a closed container, but now you can put anything you want into the container. But it isn't that easy. I want to measure two different liquids that a present in the container, water and oil.
 
Here are the requirements:
1. Monitor a container that is between 10-15 feet tall and 10 feet in diameter
2. Report the whole volume of liquid in the container
3. Report the amount of water, or water level
4. Report how much total oil is present
5. Constantly measure changes
6. Report back with an accuracy of about a 1/10th of a gallon. (or as accurate as possible)

 
 
I have a few ideas, but I don't want to contaminate early ideas with my own.

 
 
There is not right or wrong answer, so give it a shot.

 
 
Cabe


Check out some other challenges:
Design Challenge : relay spike protection
Design Challenge : The Amateur Fireworks Show
Thought Experiment; Detecting Distance
  • Sign in to reply
  • Cancel
  • gordonmx
    0 gordonmx over 15 years ago

    If the container is a cylinder with a fixed diameter, you can meaure the thickness of each layer of liquid (assuming they seperate), but to be within 1/10th of a gallon accuracy would mean you must be able to accurately a measure thickness of ~.001" for water and know the density of the oil.  At a radius of 5', a gallon of water only has a thickness of .02".

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Catwell
    0 Catwell over 15 years ago in reply to gordonmx

    Gordon,

     

    That is the challenge. To make it easier, let's say the container is over 3/4 of the way filled, but the amounts of the various liquids is not set.

     

    Thoughts?

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    Put it in a container with a clear section, put a measure up the side and once the liquids have settled read off the values?

    Done and dusted image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Catwell
    0 Catwell over 15 years ago in reply to e14 Contributor

    Tom,

     

    That is really not an option. The container is too large, and the contents of the container change quite regularly. I want to monitor the vat 24/7 with constant precision. And hiring a guy to "eyeball" the levels seems like it may lead to inaccurate results.

     

    Have any other ideas from an EDE viewpoint?

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Lotfi_G
    0 Lotfi_G over 15 years ago

    A possible solution could be the  measurment of resistivity change using a vertically inserted small  electrodes from the top of the container  (controlled by a motorised  system allowing a fine control and measurment of the level of insertion  of the electrodes within the container).

    We will notice a resistivity change when crossing interfaces between air, liquid1 and liquid 2.

     

    An  enhancement of this solution could be to use a laser telemeter from the  top to measure height of the the two liquids togheter.... when this  level changes we control the electrodes system at the interface between  liquid 1 and liquid 2 so that we avoid that the electrodes system be  continiously moving up down and down up for  real time measurments. It  just needs to be moved to monitor the liquids interface height change.

     

    Lotfi

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Catwell
    0 Catwell over 15 years ago in reply to Lotfi_G

    Lotfi,

     

    I like the laser solution, less moving parts. If the laser was turned on from the top, how would you measure the lower liquids level? Would there be two bounceback signals from the various liquids?

     

    And if the top liquid is dense oil, the laser may not penetrate enough to bounce back from the second level.

     

     

    Is ultrasonic an option?

     

    Cabe