Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum High Speed Asynchronous Counter Design?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 502 subscribers
  • Views 601 views
  • Users 0 members are here
  • microchip
  • fpga
  • Design
  • development
  • mcu
  • programmable_logic
Related

High Speed Asynchronous Counter Design?

e14 Contributor
e14 Contributor over 15 years ago

Does anyone have any sugestions as to what hardware I should use for a 100MHz + asynchronous counter design. The pulses will be about 1ns wide so may need broadening and could occur with a 2ns interval occasionally (yes I know that is 500MHz but this is for stats so missing the odd pulse is not critical).

 

Even at 100MHz we are beyond CMOS so do I need to look at CPLD's or do I need to go up to a fast FPGA?

Any other ideas?

 

Thanks

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    I would think that FPGA would be the way to go (though if this is all you are doing then it way be considered by some to be a 'waste' of the rest of the resource on a high-end fpga!

    I expect a CPLD may cope at the lower-end but towards the higher end (500Mhz) it would probably struggle, though you may be able to find a more capable high end one. I recommend you have a look at what is available on the market - I expect your primary consideration would be the 'speed-grade' of the devices (though be warned this has a DIFFERENT meaning for FPGAs than it does for CPLD devices.

     

    I hope this helps

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 15 years ago

    Consider a prescaler - here's how to build one: www.siliconchip.com.au/cms/A_107676/article.html

     

    After that you can use a PIC !

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to michaelkellett

    Thanks Michael, I should have thought about ECL. That design is very useful. The 8 bit counter is now obsolete but there is an alternative - MC100EP016AFAGMC100EP016AFAG that is actually a bit faster.

    Thank you for your help.