Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Precision 1 sec. timer needed -can you help?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 504 subscribers
  • Views 441 views
  • Users 0 members are here
Related

Precision 1 sec. timer needed -can you help?

cityswift
cityswift over 15 years ago

Hi - I need a low power timer which will produce a 1 second pulse or a 1Hz square wave with an accuracy of better than 0.1% over a range 0 to 30 degees C.  Can anyone suggest a chip or module or circuit or application note that will provide this? Thanks Dave Tedd. image

  • Sign in to reply
  • Cancel

Top Replies

  • lpetacchi
    lpetacchi over 15 years ago +1
    Hi, I would go for the venerable '4060 and a 32768Hz resonator. You have to add a F/F to get 2^15 division ratio. Accuracy is limited mainly by resonator, so 1000ppm is easily met.
  • lpetacchi
    0 lpetacchi over 15 years ago

    Hi,

    I would go for the venerable '4060 and a 32768Hz resonator. You have to add a F/F to get 2^15 division ratio. Accuracy is limited mainly by resonator, so 1000ppm is easily met.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • cityswift
    0 cityswift over 15 years ago in reply to lpetacchi

    Hi Thanks for that -have ordered the bits and will let you know how I get on.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Eavesdropper
    0 Eavesdropper over 15 years ago

    I was going to suggest the same thing! The 4060B!

     

    image

     

    E