Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum PIC18F67J60 - Clock config.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 503 subscribers
  • Views 484 views
  • Users 0 members are here
Related

PIC18F67J60 - Clock config.

KennyMillar
KennyMillar over 15 years ago

Hello,

 

I hope someone can point out where I am going wrong with this....

 

I'm trying to develop a product containing a PIC18F67J60-I/PTPIC18F67J60-I/PT processor, using MPLAB and C18.

I am supply a 25MHz clock from an external source, connected to OSC1 (Pin 39)

 

The config bits are set like this:

#pragma config FOSC = EC, FOSC2 = ON, FCMEN = OFF, IESO = OFF, DEBUG=OFF
#pragma config WDT = OFF, WDTPS = 32768
#pragma config STVR = ON, XINST=ON
#pragma config CP0 = OFF
#pragma config ETHLED = OFF

 

and my main function is this simple test routine (it's not the final use!)

void main(void)
{
// Board specific setup
// tbd
OSCCON = 0X02;
TRISA = 0x00;

while(1)
{
  PORTA = 0;
  PORTA = 0xff;
}
}

 

I believe I should be getting clk/4 out on the OSC2 (pin 40) -  but it is idle, and the pins on PORTA are not toggling, so I don't think the clock config is correct.

 

Can anyone see why this simple project isn't working ?

I have the required capacitors on the VDDCORE pin and ENVREG is tied to VDD (3.3v)

 

For the curious, here is a screen dump of the clock on pin OSC1

image

  • Sign in to reply
  • Cancel
Parents
  • gbrettell
    0 gbrettell over 15 years ago

    Have you tried using an external generator with a square wave using a 0v ~ 3.3V signal level?  Your clock signal in the image seems to be floating too high above ground (perhaps?).   <just a thought>

     

    Gregory

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • KennyMillar
    0 KennyMillar over 15 years ago in reply to gbrettell

    Thanks that was good advice.

    Indeed I slowed my clock generator down to 2MHz and was getting a lovely squarwave which did drop to 0v, but it made no difference.

    I have however found the problem - this device requires a pullup on MCLR which previous pics I had used did not.

    I've added this pull up and now it works beautifully at 25Mhz with the clock shown above.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • gbrettell
    0 gbrettell over 15 years ago in reply to KennyMillar

    Glad to hear you found the problem.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • gbrettell
    0 gbrettell over 15 years ago in reply to KennyMillar

    Glad to hear you found the problem.